Parallel shaft gear motors are the standard configuration in the industry. However, right angle gear motors are gaining popularity for its ability to minimize the footprint of a machine, such as a conveyor. Another factor that should be considered is the type of gears used in the gearhead. While worm gear technology is popular, its gear efficiency can vary from 50~90% depending on gear ratio. On the other hand, hypoid gear technology keeps its efficiency at 80~95% regardless of gear ratio. Higher gear efficiency allows more torque to be transferred from the motor to the load shaft, and sometimes allows even smaller motors to be used.
An ideal application example is shown below where a parallel shaft gear motor is installed on the side of a belt conveyor. Notice how the motor and gearhead protrudes out from the conveyor. This increases the footprint of the machine and can present a safety issue. Also, additional components, such as couplings and mounting plates, are necessary for installation.
CHALLENGE: Improve efficiency & minimizing equipment footprint
Conventional Equipment: An AC induction motor is installed on the conveyor with a parallel shaft gearhead and a coupling mechanism. An inverter (VFD) is typically used for speed control (not shown).
Problems with Conventional Equipment:
SOLUTION: BMU Series brushless motor + JH gearhead + AC input driver
Use a compact and high power
Advantages offered by BMU Series:
RESULT: reduced labor hours by using fewer parts
Read the next post to see how much mass can be reduced by switching to brushless motors.
Also: