Engineering Notes by Oriental Motor

Welcome to Oriental Motor's "Engineering Notes" Blog:

Products and technology are only valuable when coupled with skilled people and services to support them. ORIENTAL MOTOR U.S.A. CORP. has dedicated over 33 years to establishing a service and support system to better serve customers. It is our goal to provide the best product and service from the design phase, through the sale and beyond.

Our blog will feature:

  • Introductions to New Products and Technology
  • Application Examples, Improvements and Problem Solving
  • Tips and Recommendations for Motor Selection, Installation and Use

Torque Limit Application Example - Bottle Capping with BLDC Motors (VIDEO)

Posted by Johann Tang on Feb 15, 2019 1:00:00 PM

For applications where torque needs to be limited, an external mechanical torque limiter is typically required in addition to the motor system.  When the torque exceeds the limit, the torque limiter will either decouple the load or limit the torque by slipping.  An electric motor system's built-in torque limit function can simplify machine designs by eliminating this extra component.

Read More

Topics: Torque Limit, BLE2 Series, Brushless motors, Capping, VIDEOS, Speed Control, Closed-Loop Feedback Control, Gear motor

Improve Gripping Operation with Multiple Torque Limit Settings (VIDEO)

Posted by Johann Tang on Jan 15, 2019 1:00:00 PM

Robotic grippers are typically used to grip parts for transport.  The driving force behind a gripper can be pneumatic, hydraulic, or electric.  Which type is best for gripping?

Read More

Topics: VIDEOS, Brushless motors, BLE2 Series, Gripper, Torque Limit, Robotics, Closed-Loop Feedback Control, Digital Data Setting

Shorten Design Cycles for Mobile Robot Applications With Built-in Features & Functions

Posted by Johann Tang on Dec 15, 2018 12:00:00 PM

In the market of electric motors, there are products designed for general purpose applications, and there are motors designed for specialized applications, such as automated guided vehicles (AGVs) or autonomous mobile robots (AMRs).  While standard, general purpose motors work for most applications such as factory automation, sometimes, it may help shorten your design cycle by going with a motor system that already offers the features that you are planning to implement into your design.  In this post, we will summarize some of these features.

Read More

Topics: Closed-Loop Feedback Control, Speed Regulation, Gear motor, Brushless motors, AGV, AMR, Robotics, Flat Hollow Shaft Gearhead, Speed Control, BLV Series, Vector Control, Low Battery Operation, Motor Sizing

Easily Synchronize Speeds of Multiple Motors (VIDEO)

Posted by Johann Tang on Oct 15, 2018 9:00:00 AM

There are a variety of ways to synchronize the speed of multiple motors.  In this blog post, we will explain another advantage of using brushless motors systems, which is its ability to set speeds accurately and be able to synchronize speeds on multiple axes easily .  Brushless motors utilize built-in hall-effect sensors to regulate speed.  Even if the load, input voltage, or temperature fluctuates, the speed regulation will always be under +/-0.2% or better.

Read More

Topics: Speed Synchronization, Conveyor, Digital Data Setting, Labeling, AC Motors, Brushless motors, IP66, Right Angle Shaft Gearhead, Closed-Loop Feedback Control, Parallel Shaft Gearhead, BMU Series, Speed Control, VIDEOS

Designing Lighter Equipment by Reducing Motor Mass

Posted by Johann Tang on Oct 1, 2018 8:32:18 AM

With the growing popularity of efficient brushless motors, replacing AC motors with these motors brings several advantages.  In this blog post, we will uncover one of the advantages that can benefit lighter and compact equipment designs.  If we just look at the motors, brushless motors are much more power efficient than AC induction motors.  This means a smaller brushless motor can do the work of a bigger AC motor.  With recent trends in efficiency, brushless motors should be considered during the motor selection process for new designs.

Read More

Topics: AC Motors, Gear motor, Conveyor, Brushless motors, Parallel Shaft Gearhead, BMU Series, VIDEOS

Minimize Machine Footprint with Right Angle Gear Motors (VIDEO)

Posted by Johann Tang on Oct 1, 2018 8:31:15 AM

Parallel shaft gear motors are the standard configuration in the industry.  However, right angle gear motors are gaining popularity for its ability to minimize the footprint of a machine, such as a conveyor.  Another factor that should be considered is the type of gears used in the gearhead.  While worm gear technology is popular, its gear efficiency can vary from 50~90% depending on gear ratio.  On the other hand, hypoid gear technology keeps its efficiency at 80~95% regardless of gear ratio.  Higher gear efficiency allows more torque to be transferred from the motor to the load shaft, and sometimes allows even smaller motors to be used.

Read More

Topics: Brushless motors, AC Motors, Gear motor, Conveyor, Hypoid Gear, Right Angle Shaft Gearhead, Worm Gear, Spur Gear, Helical Gear, Parallel Shaft Gearhead, BMU Series, VIDEOS

Get Updates