Engineering Notes by Oriental Motor

Welcome to Oriental Motor's "Engineering Notes" Blog:

Products and technology are only valuable when coupled with skilled people and services to support them. ORIENTAL MOTOR U.S.A. CORP. has dedicated over 33 years to establishing a service and support system to better serve customers. It is our goal to provide the best product and service from the design phase, through the sale and beyond.

Our blog will feature:

  • Introductions to New Products and Technology
  • Application Examples, Improvements and Problem Solving
  • Tips and Recommendations for Motor Selection, Installation and Use

Torque Limit Application Example - Bottle Capping with BLDC Motors (VIDEO)

Posted by Johann Tang on Feb 15, 2019 1:00:00 PM

For applications where torque needs to be limited, an external mechanical torque limiter is typically required in addition to the motor system.  When the torque exceeds the limit, the torque limiter will either decouple the load or limit the torque by slipping.  An electric motor system's built-in torque limit function can simplify machine designs by eliminating this extra component.

Read More

Topics: Torque Limit, BLE2 Series, Brushless motors, Capping, VIDEOS, Speed Control, Closed-Loop Feedback Control, Gear motor

Improve Gripping Operation with Multiple Torque Limit Settings (VIDEO)

Posted by Johann Tang on Jan 15, 2019 1:00:00 PM

Robotic grippers are typically used to grip parts for transport.  The driving force behind a gripper can be pneumatic, hydraulic, or electric.  Which type is best for gripping?

Read More

Topics: VIDEOS, Brushless motors, BLE2 Series, Gripper, Torque Limit, Robotics, Closed-Loop Feedback Control, Digital Data Setting

Shorten Design Cycles for Mobile Robot Applications With Built-in Features & Functions

Posted by Johann Tang on Dec 15, 2018 12:00:00 PM

In the market of electric motors, there are products designed for general purpose applications, and there are motors designed for specialized applications, such as automated guided vehicles (AGVs) or autonomous mobile robots (AMRs).  While standard, general purpose motors work for most applications such as factory automation, sometimes, it may help shorten your design cycle by going with a motor system that already offers the features that you are planning to implement into your design.  In this post, we will summarize some of these features.

Read More

Topics: Closed-Loop Feedback Control, Speed Regulation, Gear motor, Brushless motors, AGV, AMR, Robotics, Flat Hollow Shaft Gearhead, Speed Control, BLV Series, Vector Control, Low Battery Operation, Motor Sizing

Choosing the Right Type of Stepper Motor for Your Application (VIDEOS)

Posted by Johann Tang on Nov 12, 2018 8:30:00 AM

Stepper motors are popular for their ability to position accurately as well as their ease of use.  Both the amount of rotation and the speed are controlled easily with the same digital square wave pulse signal.  Unlike servo motors, stepper motors do not need an encoder to operate.  Example applications of stepper motors are CNC machines, index tables, robotics, scanners, and more recently, 3D printers.

Read More

Topics: Stepper Motors, Motor Selection, Position Control, High Resolution, Indexing Operation, Reciprocating Motion, PKP Series, 2-Phase, 5-Phase, Closed-Loop Feedback Control, Electromagnetic Brake, Gear motor, VIDEOS

Easily Synchronize Speeds of Multiple Motors (VIDEO)

Posted by Johann Tang on Oct 15, 2018 9:00:00 AM

There are a variety of ways to synchronize the speed of multiple motors.  In this blog post, we will explain another advantage of using brushless motors systems, which is its ability to set speeds accurately and be able to synchronize speeds on multiple axes easily .  Brushless motors utilize built-in hall-effect sensors to regulate speed.  Even if the load, input voltage, or temperature fluctuates, the speed regulation will always be under +/-0.2% or better.

Read More

Topics: Speed Synchronization, Conveyor, Digital Data Setting, Labeling, AC Motors, Brushless motors, IP66, Right Angle Shaft Gearhead, Closed-Loop Feedback Control, Parallel Shaft Gearhead, BMU Series, Speed Control, VIDEOS

Get Updates