Engineering Notes by Oriental Motor

Stepper Motor Basics: PM vs VR vs Hybrid

[fa icon="calendar"] Jan 8, 2021 10:15:53 PM / by Johann Tang

Johann Tang

There are three main types of stepper motors available in the market: PM (permanent magnet) type, VR (variable reluctance) type, and hybrid type.  What are the differences, which one should you use, and how do they work?

Let's quickly review what a stepper motor does.  Stepper motors rotate in specific increments of "steps" without encoder feedback or complicated PID loops.  Rotation amount and speed are easily controlled by the number of pulses and frequency, and a stepper motor offers highly repeatable stop accuracy at ±3 arc minutes (±0.05°).  Holding torque is generated without an electromagnetic brake when a stepper motor is powered but at standstill.  They are ideal for cost-sensitive applications where motors need to stop accurately and provide holding torque.

 

Stepper motor moves in increments of steps

 

The design of a stepper motor affects its characteristics.  In the next few minutes, I will introduce the three types of stepper motors in the market and why one is preferred over the others.

 

PM "Permanent Magnet" Type 

This is a stepper motor whose rotor is made from two permanent magnet rotors which are slightly offset from each other.  The permanent magnet is axially magnetized; meaning that the north and south poles alternate and are on the same axis as the motor shaft.  When current is applied to windings, poles on the stator are magnetized and align with the opposite poles from the permanent magnet rotor.  For example, north poles would align directly across from south poles. 

A widely used PM type stepper motor is the 2-phase claw type as shown below.

 

Permanent magnet type stepper motor construction

 

The image below shows a rotor and a stator in which a current is applied so that the A1 pole is magnetized to the south pole and the A2 pole is magnetized to the north pole, therefore attracting the opposite poles from the rotor's permanent magnets.  If the current is switched from phase A to phase B to magnetize B1 to the south pole and B2 to the north pole, the rotor would rotate by 90° in the clockwise direction. 

 

Permanent magnet stepper motor simplified operation

 

The step angle is represented as follows using the number of poles of the rotor (Np) and the number of phases (Nphase).  If the number of poles or the number of phases increase, the step angle would decrease.  However, as the number of poles increases, the magnetic force and torque also become weaker.  

 

Resolution formula for PM type stepper motors Stepper motor: 8-pole rotor vs 16-pole rotor

 

A PM type stepper motor is simple in construction and inexpensive to manufacture.  The permanent magnets allow PM type stepper motors to output higher torque.  However, high speed performance is limited due to large loss during rotation.  A PM type stepper motor is often used for simple positioning since it's resolution tend to be larger than other types (ie: 3.6° or bigger).  For higher resolution, half-stepping or microstepping is recommended.  With microstepping, the driver's ability to control current precisely at each phase becomes increasingly important in determining the motor's repetitive position accuracy.  Another difference is that PM type stepper motors uses constant voltage drivers, which are more difficult to use than constant current chopper drivers.

 

VR "Variable Reluctance" Type

This is a stepper motor which provides teeth  on the rotor and stator where the magnetic forces are concentrated.  It offers the simplest design out of the three types discussed here.  The image below shows a 3-phase VR type stepper motor with 8 poles and 12 slots.  A ferromagnetic material, such as iron, is used for most magnetic cores because of its abundance on earth and its ability to pass magnetic flux easily.  A VR type stepper motor has no magnets, which means it cannot output holding torque or detent torque at standstill.

 

Variable reluctance type stepper motor construction

 

The below image shows an example of a 4-pole, 6-slot VR type stepper motor.  The "teeth" on the rotor are attracted to the magnetized poles on the stator.  The stator poles on each side of the rotor is magnetized north and south by winding the poles in reverse.

In the images below, we show a "Phase B excited" state on the left.  In this condition, the closest teeth from the rotor will align themselves to the nearest magnetic pole on the stator.  The rotor will rotate counterclockwise 30° until the teeth are aligned across each other (see "Stop position of phase B").  Now, when phase C is excited in the same way, the rotor will rotate 60° until the teeth are aligned with phase C.

 

Phase B excited Stop position of phase B Stop Position of phase C
Rotor and stator of a VR type stepper motor

 

An advantage of the VR type stepper motor is that there is no need to change the polarity of the stator poles, so that its drive circuitry can be simplified.  Its disadvantage is its inability for fine torque control since torque is proportional to the square of the current instead of to the current.  However, since it does not use permanent magnets, its high speed performance is better than a PM type stepper motor.

The step angle of the VR type stepper motor is represented in the following formula.  Np is the number of teeth of a rotor, and Nphase is the number of phases.  For finer resolutions, it's effective to increase of the number of teeth of the rotor.  However, if the number of stator slots are also increased, the structure becomes very complicated to manufacture.  The image below shows a 50-teeth rotor and stator design.  This is a 4-phase stepper motor where the coil is divided into 4 sets.  Inputting Np = 50 and Nphase = 4 would result in a step angle of 1.8°.

 

Resolution formula for VR type stepper motors

Toothed rotor and stator from a VR type stepper motor

 

VR type stepper motors have been around for a long time.  These motors have less torque drop-off at higher motor speeds, so they are often a better choice than PM type stepper motors in mid to high speed applications.  However, they are known to produce more noise, so their application range is limited.  VR type stepper motors are less common than PM type stepper motors in the market.

 

Hybrid Type Stepper Motor

A "hybrid" type stepper motor combines the design and advantages from both permanent magnet type and variable reluctance type stepper motors.  Therefore, a hybrid type stepper motor uses both the permanent magnet rotor as well as a toothed rotor and stator in their design.  With strong permanent magnets, toothed rotor, toothed stator, and a tiny air gap, a hybrid type stepper motor is able to focus the magnetic flux better than the other two types.  Low loss is achieved by stacking magnetic steel laminations that can easily pass the magnetic flux.

 

Hybrid type stepper motor construction

 

The construction of a hybrid type stepper motor starts with two rotor cups (Rotor 1 and Rotor 2) and a strong rare earth permanent magnet which is axially magnetized.  Two ball bearings mount the rotor into the motor casing.  There are either 50 teeth (1.8° per step) or 100 teeth (0.9° per step) on the rotors.  One rotor is magnetized as the north pole, and one rotor is magnetized as the south pole.  Each tooth on the rotor cups becomes a magnetic pole.  

In the 2 images below, we show a top down view of the two rotors; starting with the north pole rotor on top.  The two rotor cups are in different colors.  Red is the north pole rotor, and blue is the south pole rotor.  

 

Stepper motor rotor cups offset by 3.6°

Stepper motor: phase excitation and teeth arrangement

 

Since there are 50 teeth, the full pitch is 7.2°.  The two rotor cups are offset by a half pitch (3.6°) so the south pole teeth from rotor 1 line up in between the north pole teeth from rotor 2.  From a cross-sectional view of the rotor, you can clearly see that the north and south pole teeth are alternating because of the offset of the two rotor cups.  When the windings are energized or excited by the driver, the stator poles turns into electromagnets, and the permanent magnet rotor follows them by both a pull and push effect and stops at fixed increments.  The north poles from the stator will attract the south poles from the rotor, and vice versa.

 

Stator from a hybrid type stepper motor

 

There are eight stator poles in the stator.  When windings are wound to the main poles and a current is applied, each pole is magnetized to the north pole or the south pole.  Direction of current can determine the magnetic polarity.  When excited, two poles at opposite sides have the same polarity, and two poles positioned at 90° from these poles have the opposite polarity.  The main poles excited together are called "phases" and can be divided into two phases (phase A and phase B).  This is why it's called a "two-phase" stepper motor.

 

Formula to calculate step angle of hybrid type stepper motors

 

The step angle of a hybrid type stepper motor is in inverse proportion to the number of small teeth on the rotor ZR and the number of phases n.  The denominator 2 indicates that the main poles of the stator can be configured into two states, north pole and south pole.  This is a fundamental design difference between VR type and hybrid type stepper motors.

 

Teeth Arrangement Offset Phase A Excited Phase B Excited
Teeth arrangement offset between rotor and stator Stepper motor: phase A excited Stepper motor: phase B excited

 

The reason why hybrid type stepper motors rotate 1.8° per step is that the motor only moves a quarter of a tooth pitch per step due to the geometric design between the rotor and stator.  When phase A is excited as the south pole and its stator teeth are directly aligned with the north pole teeth from the rotor, the stator teeth of phase B are actually offset from the teeth of the rotor by 1.8°.  This is called the teeth arrange offset and is the reason why a two-phase hybrid type stepper motor rotates 1.8 ° per step.

For a 0.9° per step stepper motor, both the rotor teeth need to increase to 100.  Anything more than 100 teeth is quite difficult to manufacture.  

With hybrid type stepper motors, high torque can be obtained by the rare earth permanent magnets while high resolution obtained by the small teeth is maintained.  Also, the relationship between current and torque is close to proportional; making it easier to control than a VR type stepper motor.  Hybrid type stepper motors can also achieve higher resolution (ie: 0.72° per full step / 500 steps per revolution).  Even higher resolutions can be achieved by microstepping.  

 

Summary

  • PM (Permanent Magnet) Type: uses permanent magnets, moderate torque, low to mid-speed
  • VR (Variable Reluctance) Type: toothed rotor/stator, low torque, mid to high speed
  • Hybrid Type: combines permanent magnets and teeth, good combination of torque and speed

The most popular stepper motors in the market are the hybrid type as it offers the best performance albeit at a higher cost.  Hybrid stepper motors will work well for most applications while permanent magnet or variable reluctance stepper motors are limited to certain applications.  Stepper motor drivers are becoming increasingly smarter in recent years due to their technological improvements in functions, distributed control, and ease of programming.  Gearheads and closed-loop feedback can be added to the stepper motor to expand its range of applications.  Working with a manufacturer that can provide all the necessary components and training can make life easier.  

 

Interested in learning more? 
Learn more about stepper motors fundamentals from our technical articles and white papers. 

White Papers - Stepper Motors Fundamentals

 

Please meet our high torque hybrid stepper motors!

New call-to-action

 

Topics: Stepper Motors, Motion Control Basics

Johann Tang

Written by Johann Tang

Johann Tang is a Product Specialist at Oriental Motor USA Corp. with 20+ years of experience in sales, technical application support, and training of various types of fractional horsepower electric motors, gear motors, actuators, drivers, and controllers. Feel free to ask him questions on Linkedin.

    Subscribe Here!

    Recent Posts

    New call-to-action
    Product Guide