Engineering Notes by Oriental Motor

Welcome to Oriental Motor's "Engineering Notes" Blog:

Products and technology are only valuable when coupled with skilled people and services to support them. Since 1978, ORIENTAL MOTOR U.S.A. CORP. has been building a service and support system to better serve customers. It is our goal to provide the best product and service from the design phase, through the sale and beyond.

Our blog will feature:

  • Introduction to new products and technologies
  • Motion control basics and application examples
  • Tips for motor selection, programming, and troubleshooting

 

Technical Manual Series: Technologies Used with Brushless Motors (Part II)

Posted by Johann Tang on Oct 29, 2021, 7:55:31 PM

This is a continuation of the blog post, "Technologies Used with Brushless Motors".  In this section, we explain the efficiency aspect of brushless motors and compare them to AC motors.

Read More

Topics: Speed Control, BLDC Motors, Technical Manual Series

Technical Manual Series: Technologies Used with Brushless Motors (Part I)

Posted by Johann Tang on Aug 31, 2021, 10:12:33 PM

Brushless motors have characteristics that make them excellent motors for speed control.  In this section, we will explain the technologies that enhance the performance of these motors. 

Read More

Topics: Speed Control, BLDC Motors, Technical Manual Series

Technical Manual Series: Brushless Motor Current Control Method

Posted by Johann Tang on Aug 1, 2021, 2:55:28 AM

Brushless motors have different methods of controlling current flow depending on the drive system.  In addition, to control the rotation speed and generated torque, it is necessary to control the amount of the motor current.  Here, we will explain the PWM method for controlling the motor current.

Read More

Topics: Speed Control, BLDC Motors, Technical Manual Series

Technical Manual Series: Brushless Motor Drive Systems and Motor Torque

Posted by Johann Tang on Aug 1, 2021, 2:47:49 AM

In this post, we will explain how the two drive systems, square wave drive and sine wave drive, can affect motor torque performance.

Read More

Topics: Speed Control, BLDC Motors, Technical Manual Series

Technical Manual Series: Brushless Motor Drive Systems

Posted by Johann Tang on Aug 1, 2021, 2:45:15 AM

There is a close relationship between the drive system and brushless motor characteristics, and various methods have been used to improve the controllability and characteristics of motors.  In this post, we will explain two typical drive systems: square wave drive and sine wave drive.

Read More

Topics: Speed Control, BLDC Motors, Technical Manual Series

Technical Manual Series: Main Components of Brushless Motors

Posted by Johann Tang on Jun 25, 2021, 8:55:05 PM

In part 4, we will explain the main components of brushless motors: feedback, magnetic field, and permanent magnets.

Read More

Topics: Speed Control, BLDC Motors, Technical Manual Series

Technical Manual Series: Brushless Motor Structure and Rotation Principles

Posted by Johann Tang on Jun 24, 2021, 7:47:39 PM

In part 3, we will explain the differences in the structure and rotation principles of brushless motors, and compare them to brushed DC motors and AC motors.

Read More

Topics: Speed Control, BLDC Motors, Technical Manual Series

Technical Manual Series: Brushed DC Motor Structure and Principles

Posted by Johann Tang on May 28, 2021, 9:00:00 AM

This is part 2 of the Technical Manual Series for brushless motors, which explains the structure and operating principles for brushed motors for comparison.  We will explain brushless motors next.

Read More

Topics: BLDC Motors, Technical Manual Series

Technical Manual Series: Types of Brushless Motors

Posted by Johann Tang on May 21, 2021, 9:00:00 AM

This is part 1 of the Technical Manual Series for brushless motors, which explains the three main types of brushless motors: inner rotor type, outer rotor type, and disk rotor type.

Read More

Topics: Speed Control, VIDEOS, BLDC Motors, Technical Manual Series

    Subscribe Here!