Engineering Notes by Oriental Motor

Welcome to Oriental Motor's "Engineering Notes" Blog:

Products and technology are only valuable when coupled with skilled people and services to support them. Since 1978, ORIENTAL MOTOR U.S.A. CORP. has been building a service and support system to better serve customers. It is our goal to provide the best product and service from the design phase, through the sale and beyond.

Our blog will feature:

  • Introduction to new products and technologies
  • Motion control basics and application examples
  • Tips for motor selection, programming, and troubleshooting

 

Coordinated Robots Bring Precision and Flexibility to Automated Bottle Capping

Posted by Johann Tang on Apr 27, 2026, 8:00:00 PM

Coordinated Robots Bring Precision and Flexibility to Automated Bottle Capping
8:50

As packaging lines face increasing pressure to run faster, handle more variants, and fit into tighter footprints, automation strategies must balance precision, flexibility, and size. One effective approach is the coordinated use of compact robots integrated with machine vision - an architecture well-suited for highly repeatable tasks like bottle handling and capping.

Read More

Topics: Robotics, VIDEOS, Application Examples, Food & Packaging, Bottle Capping, Product Demos, Factory Automation

Advancing Conveyor Design and Performance with Brushless DC Motors

Posted by Johann Tang on Jan 31, 2025, 8:00:00 PM

Advancing Conveyor Design and Performance with Brushless DC Motors
5:38

AC induction motors are the workhorses that power many types of conveyors to transport materials.  However, there's a smaller but mightier type of motor that can help enhance the design and performance of conveyors for many industries.

Read More

Topics: Speed Control, VIDEOS, BLDC Motors, Application Examples, Product Introductions, Food & Packaging, Grip Conveyors, Conveyors, Factory Automation

Case Study: How a Compact Electric Gripper Can Help with Articulated Robots

Posted by Johann Tang on May 31, 2024, 8:45:00 AM

Case Study: How a Compact Electric Gripper Can Help with Articulated Robots
14:17

An end effector, such as an electric gripper, is an essential part of industrial robots. More importantly, using the right gripper for the load being transferred prevents damage while improving automation efficiency.  In this article, we share how one system integrator has successfully adopted an electric gripper for one of their articulated robots.

Read More

Topics: Robotics, Absolute Positioning, Alphastep Hybrid Control, Linear Actuators, VIDEOS, Application Examples, Medical, Food & Packaging, Case Studies, Factory Automation

Why Brushless Motors Make Sense for Conveyors

Posted by Johann Tang on Aug 31, 2023, 6:53:31 PM

In today's fast-paced industrial landscape, the role of conveyors has become more crucial than ever. These systems efficiently move materials, products, and goods for numerous industries, from labeling and packaging to warehousing and distribution.  While many types of motors can be used in conveyors, this article highlights a few reasons why brushless motors should be a primary choice for conveyor applications.

Read More

Topics: Speed Control, VIDEOS, BLDC Motors, Application Examples, Food & Packaging, Semiconductors, Conveyors, Factory Automation

Case Study: Using Agricultural Automation to Improve Production Efficiency

Posted by Johann Tang on Jul 19, 2022, 7:57:05 PM

According to the Food and Agriculture Organization (FAO) of the United Nations, global food prices reached an all-time high in 2022.  This case study explains how a vegetable farm in Hokkaido, Japan, improved production efficiency and reduced costs by building in-house automation.

Read More

Topics: AC Motors, Speed Control, BLDC Motors, Washdown, Food & Packaging, Case Studies, Factory Automation

Motor Sizing & Selection Example: Variable Speed Belt Conveyor

Posted by Johann Tang on Dec 28, 2021, 12:00:00 PM

Many motor manufacturers offer a motor sizing tool to help with product selection, but if you don't know how to use it, you may still end up paying for it in the long run.

Read More

Topics: Speed Control, Motor Sizing, BLDC Motors, Food & Packaging, Conveyors, Factory Automation

Torque Limit Application Example - Bottle Capping with BLDC Motors

Posted by Johann Tang on Feb 15, 2019, 1:00:00 PM

For applications where torque needs to be limited, an external mechanical torque limiter is typically required in addition to the motor system.  When the torque exceeds the limit, the torque limiter will either decouple the load or limit the torque by slipping.  An electric motor system's built-in torque limit function can simplify machine designs by eliminating this extra component.

Read More

Topics: Torque Limit (Push Motion, Tension Control), Speed Control, VIDEOS, BLDC Motors, Application Examples, Food & Packaging, Bottle Capping

Easily Synchronize Speeds of Multiple Motors

Posted by Johann Tang on Oct 15, 2018, 9:00:00 AM

There are a variety of ways to synchronize the speed of multiple motors.  In this blog post, we will explain another advantage of using brushless motors systems, which is its ability to set speeds accurately and be able to synchronize speeds on multiple axes easily .  Brushless motors utilize built-in hall-effect sensors to regulate speed.  Even if the load, input voltage, or temperature fluctuates, the speed regulation will always be under +/-0.2% or better.

Read More

Topics: AC Motors, Speed Control, VIDEOS, BLDC Motors, Washdown, Application Examples, Medical, Food & Packaging, Grip Conveyors, Conveyors

Designing Smaller and Lighter Conveyors With Brushless Motors

Posted by Johann Tang on Oct 1, 2018, 8:32:18 AM

With the growing popularity of efficient brushless motors, replacing AC motors with these motors brings several advantages.  In this blog post, we will uncover one of the advantages that can benefit lighter and compact equipment designs. 

Read More

Topics: AC Motors, Speed Control, VIDEOS, BLDC Motors, Washdown, Application Examples, Medical, Food & Packaging, Grip Conveyors, Conveyors, Factory Automation

Minimize Conveyor Footprint with Right Angle Brushless Gear Motors

Posted by Johann Tang on Oct 1, 2018, 8:31:15 AM

Parallel shaft AC gear motors are the standard configuration in the industry.  However, right angle brushless gear motors are gaining popularity for their ability to minimize the footprint of a machine, such as a conveyor.  

Read More

Topics: AC Motors, Speed Control, VIDEOS, BLDC Motors, Gearheads, Application Examples, Medical, Food & Packaging, Conveyors, Factory Automation

    Subscribe Here!