Engineering Notes by Oriental Motor

Welcome to Oriental Motor's "Engineering Notes" Blog:

Products and technology are only valuable when coupled with skilled people and services to support them. Since 1978, ORIENTAL MOTOR U.S.A. CORP. has been building a service and support system to better serve customers. It is our goal to provide the best product and service from the design phase, through the sale and beyond.

Our blog will feature:

  • Introduction to new products and technologies
  • Motion control basics and application examples
  • Tips for motor selection, programming, and troubleshooting

 

Advancing Conveyor Design and Performance with Brushless DC Motors

Posted by Johann Tang on Jan 31, 2025, 8:00:00 PM

Advancing Conveyor Design and Performance with Brushless DC Motors
5:38

AC induction motors are the workhorses that power many types of conveyors to transport materials.  However, there's a smaller but mightier type of motor that can help enhance the design and performance of conveyors for many industries.

Read More

Topics: Speed Control, VIDEOS, BLDC Motors, Application Examples, Product Introductions, Food & Packaging, Grip Conveyors, Conveyors, Factory Automation

Explainer: How to Synchronize Speeds Between Multiple Motors with One Potentiometer

Posted by Johann Tang on Dec 31, 2024, 12:00:00 PM

Explainer: How to Synchronize Speeds Between Multiple Motors with One Potentiometer
9:41

For speed synchronization applications like a dual belt labeling conveyor, multiple motors must run at the same speed.  What is the best type of motor to use and what are the methods to achieve this?  Our application engineer set up a product demonstration to show you how this can be done with one potentiometer.

Read More

Topics: Speed Control, VIDEOS, BLDC Motors, Grip Conveyors, Conveyors, Product Demos

Improve Gripping Operation with Multiple Torque Limit Settings

Posted by Johann Tang on Jan 15, 2019, 1:00:00 PM

Robotic grippers are typically used to grip parts for transport.  The driving force behind a gripper can be pneumatic, hydraulic, or electric.  Which type is best for gripping?

Read More

Topics: Torque Limit (Push Motion, Tension Control), Robotics, Speed Control, VIDEOS, BLDC Motors, Application Examples, Medical, Grip Conveyors

Easily Synchronize Speeds of Multiple Motors

Posted by Johann Tang on Oct 15, 2018, 9:00:00 AM

There are a variety of ways to synchronize the speed of multiple motors.  In this blog post, we will explain another advantage of using brushless motors systems, which is its ability to set speeds accurately and be able to synchronize speeds on multiple axes easily .  Brushless motors utilize built-in hall-effect sensors to regulate speed.  Even if the load, input voltage, or temperature fluctuates, the speed regulation will always be under +/-0.2% or better.

Read More

Topics: AC Motors, Speed Control, VIDEOS, BLDC Motors, Washdown, Application Examples, Medical, Food & Packaging, Grip Conveyors, Conveyors

Designing Smaller and Lighter Conveyors With Brushless Motors

Posted by Johann Tang on Oct 1, 2018, 8:32:18 AM

With the growing popularity of efficient brushless motors, replacing AC motors with these motors brings several advantages.  In this blog post, we will uncover one of the advantages that can benefit lighter and compact equipment designs. 

Read More

Topics: AC Motors, Speed Control, VIDEOS, BLDC Motors, Washdown, Application Examples, Medical, Food & Packaging, Grip Conveyors, Conveyors, Factory Automation

    Subscribe Here!