---
title: Torque Limit Application Example - Bottle Capping with BLDC Motors
description: For applications where torque needs to be limited, an external mechanical torque limiter is typically required in addition to the motor system.  When the torque exceeds the limit, the torque limiter will either decouple the load or limit the torque by slipping.  An electric motor system's built-in torque limit function can simplify machine designs by eliminating this extra component.
image: https://blog.orientalmotor.com/hubfs/Capper%20example.jpg
---

[![Oriental Motor U.S.A. Corp.](https://blog.orientalmotor.com/hs-fs/hubfs/OM-logo-200px.jpg?width=200&height=47&name=OM-logo-200px.jpg)](https://www.orientalmotor.com/index.html)

- <https://blog.orientalmotor.com>
- [Products](https://www.orientalmotor.com/products/index.html)
- [Motor Sizing](https://www.orientalmotor.com/motor-sizing/index.html)
- [Technology](https://www.orientalmotor.com/technology/index.html)
- [FAQ](https://faq.orientalmotor.com/)
- [Contact Us](https://www.orientalmotor.com/contact/index.html)

- [Stepper Motors](https://www.orientalmotor.com/stepper-motors/index.html)
- [Servo Motors](https://www.orientalmotor.com/servo-motors/index.html)
- [Industrial Robots](https://www.orientalmotor.com/industrial-robots/index.html)
- [AC Motors & Gear Motors](https://www.orientalmotor.com/ac-motors-gear-motors/index.html)
- [Brushless DC Motors](https://www.orientalmotor.com/brushless-dc-motors-gear-motors/index.html)
- [Linear Actuators](https://www.orientalmotor.com/linear-actuators/index.html)
- [Rotary Actuators](https://www.orientalmotor.com/rotary-actuators/index.html)
- [Network Products](https://www.orientalmotor.com/network-products/index.html)
- [Cooling Fans](https://www.orientalmotor.com/cooling-fans/index.html)
- [Encoders](https://www.orientalmotor.com/encoders-sensors/index.html)

Engineering Notes

## Engineering Notes by Oriental Motor

# [Torque Limit Application Example - Bottle Capping with BLDC Motors](https://blog.orientalmotor.com/torque-limit-application-example-bottle-capping)

 \[fa icon="calendar"\] Originally posted on Feb 15, 2019, 1:00:00 PM   
Last updated on September 25, 2024 / by [Johann Tang](https://blog.orientalmotor.com/author/johann-tang)

![Johann Tang](https://app.hubspot.com/settings/avatar/8cc777610596a2b2230de2963e906c0b)

- [Tweet](https://twitter.com/share)

For applications where torque needs to be limited, an external mechanical torque limiter is typically required in addition to the motor system.  When the torque exceeds the limit, the torque limiter will either decouple the load or limit the torque by slipping.  An electric motor system's built-in torque limit function can simplify machine designs by eliminating this extra component.

 **Challenge  Design a simple and affordable bottle capper without an external torque limiter** 

![Capper example](https://blog.orientalmotor.com/hs-fs/hubfs/Capper%20example.jpg?width=243&name=Capper%20example.jpg)**Conventional Capping Machine**

---

To prevent damage to caps caused by excessive torque, a conventional capping machine tightens the bottle caps to an appropriate torque level by using an external torque limiter or magnetic clutch device.

**Problems with Conventional Capping**

---

The torque limiter or magnetic clutch and other external components are required.  This makes the machine more complicated and expensive.

 

 **Solution  Use the torque limit function of a brushless motor system to eliminate the torque limiter** 

Several of Oriental Motor's brushless motor systems feature a built-in electrical torque limit function.  This function allows the user to set a certain torque limit by a % of the rated torque, and it will regulate the torque at that level.  This function is designed for processes such as capping, pressing, or stamping.

For example, use a BLE2 Series brushless motor and driver system to eliminate the external torque limiter.  Since no external parts are required, the equipment design can be simplified, and the cost can be reduced.

![Capper with BLE2-1](https://blog.orientalmotor.com/hs-fs/hubfs/Capper%20with%20BLE2-1.jpg?width=243&name=Capper%20with%20BLE2-1.jpg)With the torque limit function, the motor system can be set up to generate a torque that does not exceed the set value as a % of the rated torque.  With the BLE2 Series, up to 16 different torque limit settings can be stored.  Other systems, such as the AZ Series stepper motors, can store up to 256 different settings.

 

![Torque limit setup with graph](https://blog.orientalmotor.com/hs-fs/hubfs/Torque%20limit%20setup%20with%20graph.jpg?width=450&name=Torque%20limit%20setup%20with%20graph.jpg)

 

**How Does It Work?**

A driver monitors feedback from the motor and regulates current and speed based on operating conditions.  Since current is proportional to torque, torque is also controlled.  Setting a torque limit basically limits the motor current.  However, the motor will keep rotating at the set torque limit even when it is stalling, and the motor can be back-driven without issues.

![BLE2 torque limit specs](https://blog.orientalmotor.com/hs-fs/hubfs/BLE2%20torque%20limit%20specs.jpg?width=450&name=BLE2%20torque%20limit%20specs.jpg)![16 torque limits](https://blog.orientalmotor.com/hs-fs/hubfs/16%20torque%20limits.jpg?width=250&name=16%20torque%20limits.jpg)

✽1: The value for the rated torque is 100%.  
 ✽2: An error up to a max. of approximately ±10% (at rated torque and rated speed) may occur between the setting value and generated torque due to the setting speed, power supply voltage,  
 or motor cable extension length.  
 ✽3: The BX II Series with a speed control range of 2∼4000 r/min is also available.

Watch this video to see how feedback control, alarm output and torque limits works with a BLE2 Series motor and driver.  Stored operation data can be changed by the front panel buttons of the driver, or by the MEXE02 support software.

| <iframe style="margin-left: auto; margin-right: auto; display: block; margin: 0px auto;" allow="accelerometer; autoplay; encrypted-media; gyroscope; picture-in-picture" xml="lang" src="https://www.youtube.com/embed/gulX1tNy4Z8?rel=0" width="560" height="315" frameborder="0" allowfullscreen></iframe> |
| --- |

 

| [![More About BLE2 Series](https://hubspot-no-cache-na2-prod.s3.amazonaws.com/cta/default/2284573/d1810b10-e027-4b6c-9ff0-9e6ab4a8c9df.png)](https://hubspot-cta-redirect-na2-prod.s3.amazonaws.com/cta/redirect/2284573/d1810b10-e027-4b6c-9ff0-9e6ab4a8c9df) | [![Watch More Videos](https://hubspot-no-cache-na2-prod.s3.amazonaws.com/cta/default/2284573/584b0b91-eaea-469a-96be-13f6701c63f9.png)](https://hubspot-cta-redirect-na2-prod.s3.amazonaws.com/cta/redirect/2284573/584b0b91-eaea-469a-96be-13f6701c63f9) |
| --- | --- |

 Topics: [Torque Limit (Push Motion, Tension Control)](https://blog.orientalmotor.com/topic/torque-limit-push-motion-tension-control), [Speed Control](https://blog.orientalmotor.com/topic/speed-control), [VIDEOS](https://blog.orientalmotor.com/topic/videos), [BLDC Motors](https://blog.orientalmotor.com/topic/bldc-motors), [Application Examples](https://blog.orientalmotor.com/topic/application-examples), [Food & Packaging](https://blog.orientalmotor.com/topic/food-packaging), [Bottle Capping](https://blog.orientalmotor.com/topic/bottle-capping)

![Johann Tang](https://app.hubspot.com/settings/avatar/8cc777610596a2b2230de2963e906c0b)

#### Written by [Johann Tang](https://blog.orientalmotor.com/author/johann-tang)

Johann Tang is a Product Specialist at Oriental Motor USA Corp. Before joining the marketing team, he spent 14 years in sales and technical application support, and he also led product training on various types of fractional-horsepower electric motors, gear motors, actuators, drivers, and controllers. If you have any questions, please feel free to use the live chat window, 1-800-GO-VEXTA (1-800-468-3982), or techsupport@orientalmotor.com, to reach our product support team. Sorry, comments have been turned off.

[\[fa icon="linkedin-square"\]Linkedin](https://www.linkedin.com/in/johanntang/)

Search

### Subscribe Here!

- Recent
- Popular
- Categories

### Lists by Topic

- [Stepper Motors (62)](https://blog.orientalmotor.com/topic/stepper-motors)
- [VIDEOS (62)](https://blog.orientalmotor.com/topic/videos)
- [Application Examples (50)](https://blog.orientalmotor.com/topic/application-examples)
- [Speed Control (48)](https://blog.orientalmotor.com/topic/speed-control)
- [BLDC Motors (47)](https://blog.orientalmotor.com/topic/bldc-motors)
- [Alphastep Hybrid Control (41)](https://blog.orientalmotor.com/topic/alphastep-hybrid-control)
- [Absolute Positioning (37)](https://blog.orientalmotor.com/topic/absolute-positioning)
- [Linear Actuators (35)](https://blog.orientalmotor.com/topic/linear-actuators)
- [AC Motors (32)](https://blog.orientalmotor.com/topic/ac-motors)
- [Robotics (26)](https://blog.orientalmotor.com/topic/robotics)
- [Motion Control Basics (20)](https://blog.orientalmotor.com/topic/motion-control-basics)
- [Gearheads (17)](https://blog.orientalmotor.com/topic/gearheads)
- [Software (17)](https://blog.orientalmotor.com/topic/software)
- [Incremental Positioning (16)](https://blog.orientalmotor.com/topic/incremental-positioning)
- [Servo Motors (15)](https://blog.orientalmotor.com/topic/servo-motors)
- [Factory Automation (14)](https://blog.orientalmotor.com/topic/factory-automation)
- [Product Introductions (14)](https://blog.orientalmotor.com/topic/product-introductions)
- [Motor Sizing (13)](https://blog.orientalmotor.com/topic/motor-sizing)
- [Conveyors (12)](https://blog.orientalmotor.com/topic/conveyors)
- [Medical (11)](https://blog.orientalmotor.com/topic/medical)
- [Network (11)](https://blog.orientalmotor.com/topic/network)
- [Food & Packaging (10)](https://blog.orientalmotor.com/topic/food-packaging)
- [Technical Manual Series (9)](https://blog.orientalmotor.com/topic/technical-manual-series)
- [Rotary Actuators/Index Tables (8)](https://blog.orientalmotor.com/topic/rotary-actuators-index-tables)
- [Stepper Drivers (8)](https://blog.orientalmotor.com/topic/stepper-drivers)
- [Encoders (6)](https://blog.orientalmotor.com/topic/encoders)
- [Troubleshooting (6)](https://blog.orientalmotor.com/topic/troubleshooting)
- [Washdown (6)](https://blog.orientalmotor.com/topic/washdown)
- [Case Studies (5)](https://blog.orientalmotor.com/topic/case-studies)
- [Grip Conveyors (5)](https://blog.orientalmotor.com/topic/grip-conveyors)
- [Semiconductors (5)](https://blog.orientalmotor.com/topic/semiconductors)
- [Product Demos (4)](https://blog.orientalmotor.com/topic/product-demos)
- [Smooth Drive (4)](https://blog.orientalmotor.com/topic/smooth-drive)
- [Torque Limit (Push Motion, Tension Control) (4)](https://blog.orientalmotor.com/topic/torque-limit-push-motion-tension-control)
- [Vertical Lifts (4)](https://blog.orientalmotor.com/topic/vertical-lifts)
- [XYZ/Cartesian/Gantry (4)](https://blog.orientalmotor.com/topic/xyz-cartesian-gantry)
- [AGV/AMR (3)](https://blog.orientalmotor.com/topic/agv-amr)
- [Bottle Capping (3)](https://blog.orientalmotor.com/topic/bottle-capping)
- [Cooling Fans (3)](https://blog.orientalmotor.com/topic/cooling-fans)
- [Service Life (3)](https://blog.orientalmotor.com/topic/service-life)
- [Laboratory (2)](https://blog.orientalmotor.com/topic/laboratory)
- [Pumps (2)](https://blog.orientalmotor.com/topic/pumps)
- [Chemical Mechanical Polishing (1)](https://blog.orientalmotor.com/topic/chemical-mechanical-polishing)
- [Wafer Handling (1)](https://blog.orientalmotor.com/topic/wafer-handling)
- [Wafer Pin Lifters (1)](https://blog.orientalmotor.com/topic/wafer-pin-lifters)

see all

### Posts by Topic

- [Stepper Motors (62)](https://blog.orientalmotor.com/topic/stepper-motors)
- [VIDEOS (62)](https://blog.orientalmotor.com/topic/videos)
- [Application Examples (50)](https://blog.orientalmotor.com/topic/application-examples)
- [Speed Control (48)](https://blog.orientalmotor.com/topic/speed-control)
- [BLDC Motors (47)](https://blog.orientalmotor.com/topic/bldc-motors)
- [Alphastep Hybrid Control (41)](https://blog.orientalmotor.com/topic/alphastep-hybrid-control)
- [Absolute Positioning (37)](https://blog.orientalmotor.com/topic/absolute-positioning)
- [Linear Actuators (35)](https://blog.orientalmotor.com/topic/linear-actuators)
- [AC Motors (32)](https://blog.orientalmotor.com/topic/ac-motors)
- [Robotics (26)](https://blog.orientalmotor.com/topic/robotics)
- [Motion Control Basics (20)](https://blog.orientalmotor.com/topic/motion-control-basics)
- [Gearheads (17)](https://blog.orientalmotor.com/topic/gearheads)
- [Software (17)](https://blog.orientalmotor.com/topic/software)
- [Incremental Positioning (16)](https://blog.orientalmotor.com/topic/incremental-positioning)
- [Servo Motors (15)](https://blog.orientalmotor.com/topic/servo-motors)
- [Factory Automation (14)](https://blog.orientalmotor.com/topic/factory-automation)
- [Product Introductions (14)](https://blog.orientalmotor.com/topic/product-introductions)
- [Motor Sizing (13)](https://blog.orientalmotor.com/topic/motor-sizing)
- [Conveyors (12)](https://blog.orientalmotor.com/topic/conveyors)
- [Medical (11)](https://blog.orientalmotor.com/topic/medical)
- [Network (11)](https://blog.orientalmotor.com/topic/network)
- [Food & Packaging (10)](https://blog.orientalmotor.com/topic/food-packaging)
- [Technical Manual Series (9)](https://blog.orientalmotor.com/topic/technical-manual-series)
- [Rotary Actuators/Index Tables (8)](https://blog.orientalmotor.com/topic/rotary-actuators-index-tables)
- [Stepper Drivers (8)](https://blog.orientalmotor.com/topic/stepper-drivers)
- [Encoders (6)](https://blog.orientalmotor.com/topic/encoders)
- [Troubleshooting (6)](https://blog.orientalmotor.com/topic/troubleshooting)
- [Washdown (6)](https://blog.orientalmotor.com/topic/washdown)
- [Case Studies (5)](https://blog.orientalmotor.com/topic/case-studies)
- [Grip Conveyors (5)](https://blog.orientalmotor.com/topic/grip-conveyors)
- [Semiconductors (5)](https://blog.orientalmotor.com/topic/semiconductors)
- [Product Demos (4)](https://blog.orientalmotor.com/topic/product-demos)
- [Smooth Drive (4)](https://blog.orientalmotor.com/topic/smooth-drive)
- [Torque Limit (Push Motion, Tension Control) (4)](https://blog.orientalmotor.com/topic/torque-limit-push-motion-tension-control)
- [Vertical Lifts (4)](https://blog.orientalmotor.com/topic/vertical-lifts)
- [XYZ/Cartesian/Gantry (4)](https://blog.orientalmotor.com/topic/xyz-cartesian-gantry)
- [AGV/AMR (3)](https://blog.orientalmotor.com/topic/agv-amr)
- [Bottle Capping (3)](https://blog.orientalmotor.com/topic/bottle-capping)
- [Cooling Fans (3)](https://blog.orientalmotor.com/topic/cooling-fans)
- [Service Life (3)](https://blog.orientalmotor.com/topic/service-life)
- [Laboratory (2)](https://blog.orientalmotor.com/topic/laboratory)
- [Pumps (2)](https://blog.orientalmotor.com/topic/pumps)
- [Chemical Mechanical Polishing (1)](https://blog.orientalmotor.com/topic/chemical-mechanical-polishing)
- [Wafer Handling (1)](https://blog.orientalmotor.com/topic/wafer-handling)
- [Wafer Pin Lifters (1)](https://blog.orientalmotor.com/topic/wafer-pin-lifters)

see all

### Recent Posts

[![New call-to-action](https://hubspot-no-cache-na2-prod.s3.amazonaws.com/cta/default/2284573/f24cd0b7-792e-4246-a809-1f6331235405.png)](https://hubspot-cta-redirect-na2-prod.s3.amazonaws.com/cta/redirect/2284573/f24cd0b7-792e-4246-a809-1f6331235405)

[![product-guide-gray-drop-shadow](https://hubspot-no-cache-na2-prod.s3.amazonaws.com/cta/default/2284573/interactive-194050460599.png)](https://blog.orientalmotor.com/hs/cta/wi/redirect?encryptedPayload=AVxigLJPhhHZN5TcBnod9k%2FVPTKbNRP7gJCxAA4NQp40LjnSRQSRqYOEZuTvQfxu6aktxbh22phGnFNgruyNBtYp9pl9bDCynwDNpxkjCz4QMvCD2lx75kr3R6cOww85OD5X5YjGxkRkobcQIl%2BqzLSdDywYVajxikKdMy0G%2F8prJzUKW3OVVoRlgQV%2ByEPJG6NKOMDTAw%2B%2BYdQkblAIJOSBxEqEyosUpaC9sh7GWypT&webInteractiveContentId=194050460599&portalId=2284573)

#### About Us

Oriental Motor offers an extensive product line-up of about 50,000 different products that provide the optimal motion system. For over a century we have concentrated on technological advancement and product design improvement. This emphasis is evident in the sophisticated devices that we market today. Oriental Motor's sales and service network is international, with offices throughout North America, Europe and Asia.

#### More Links

- [\[fa icon="caret-right"\] Home](http://www.orientalmotor.com)
- [\[fa icon="caret-right"\] About Us](http://www.orientalmotor.com/company/index.html)
- [\[fa icon="caret-right"\] Contact Us](http://www.orientalmotor.com/contact/index.html)

#### Contact Us

\[fa icon="phone"\]  1-800-GO-VEXTA (468-3982)

\[fa icon="envelope"\]  sales@orientalmotor.com

\[fa icon="home"\]  570 Alaska Avenue, Torrance CA 90503

\[fa icon="chevron-up"\]Back to top

```json
{
  "@context" : "https://schema.org",
  "@type" : "BlogPosting",
  "author" : {
    "@type" : "Person",
    "name" : "Johann Tang",
    "url" : "https://blog.orientalmotor.com/author/johann-tang"
  },
  "dateModified" : "2024-09-25T18:51:27.656Z",
  "datePublished" : "2019-02-15T18:00:00.000Z",
  "headline" : "Torque Limit Application Example - Bottle Capping with BLDC Motors",
  "image" : [ "https://blog.orientalmotor.com/hubfs/Capper%20example.jpg" ],
  "mainEntityOfPage" : {
    "@id" : "https://blog.orientalmotor.com/torque-limit-application-example-bottle-capping",
    "@type" : "WebPage"
  },
  "publisher" : {
    "@type" : "Organization",
    "logo" : {
      "@type" : "ImageObject",
      "url" : "https://blog.orientalmotor.com/hubfs/OM-brand-logo-640x83.jpg"
    },
    "name" : "Oriental Motors"
  }
}
```