Besides load torque, acceleration torque, speed, and load inertia, overlooking certain sizing parameters during the motor sizing process can literally make or break your machine.
Welcome to Oriental Motor's "Engineering Notes" Blog:
Products and technology are only valuable when coupled with skilled people and services to support them. ORIENTAL MOTOR U.S.A. CORP. has dedicated over 33 years to establishing a service and support system to better serve customers. It is our goal to provide the best product and service from the design phase, through the sale and beyond.
Our blog will feature:
- Introductions to New Products and Technology
- Application Examples, Improvements and Problem Solving
- Tips and Recommendations for Motor Selection, Installation and Use
Motor Sizing Basics Part 4 - How to Calculate Radial Load and Axial Load
Topics: AC Motors, Stepper Motors, Speed Control, Motor Sizing, Capping, BLDC Motors, Gearheads, Servo Motors, Motion Control Basics
Improve Motor Performance With Redesigned Compact BLDC Drivers
The BLH Series compact BLDC motors and drivers have been around for a long time, and there is a good reason. Customers seem to favor the combination of a highly efficient, compact motor and a light weight board type driver that is easy to use. Having a high torque, flat style hollow shaft gearhead as an option also helps in increasing torque as well as minimizing footprint.
Topics: Torque Limit (Push Motion), Robotics, Speed Control, VIDEOS, Capping, BLDC Motors, Software
Torque Limit Application Example - Bottle Capping with BLDC Motors (VIDEO)
For applications where torque needs to be limited, an external mechanical torque limiter is typically required in addition to the motor system. When the torque exceeds the limit, the torque limiter will either decouple the load or limit the torque by slipping. An electric motor system's built-in torque limit function can simplify machine designs by eliminating this extra component.
Topics: Torque Limit (Push Motion), Speed Control, VIDEOS, Capping, BLDC Motors, Application Examples