Engineering Notes by Oriental Motor

How VFD-Compatible BLDC Motors Address Common Challenges of VFD-Driven AC Motors

[fa icon="calendar"] Originally posted on Jun 30, 2026 8:58:19 PM
Last updated on July 1, 2026 / by Johann Tang

Johann Tang

How VFD-Compatible BLDC Motors Address Common Challenges of VFD-Driven AC Motors
12:52

Due to technological advancements, VFD users are no longer limited to AC motors.  Another alternative, brushless DC (BLDC) motors, is becoming increasingly popular for their ability to reduce footprint, lower power consumption, and improve performance.  We know that replacing a VFD and motor takes more work than just swapping out parts, so we came up with a simpler solution.

This article breaks down the common challenges associated with AC motors and VFDs and explains how VFD-compatible BLDC motors can address them.

Table of Contents:

  • Common Challenges with AC Motors and VFDs
  • What is a BLDC Motor?
  • How Do BLDC Motors Resolve Common Challenges of AC Motors?
  • When to Choose BLDC Motors vs. AC Induction Motors

 

Common Challenges with AC Motors and VFDs

πŸ‘Ž Space and Packaging Constraints

AC motors are not efficient and have lower power density, so they require a relatively large motor frame size and case length.  Larger motors require external cooling fans, which increase their size even more.  The VFDs themselves also require a cabinet with cooling clearance.  As machines become more compact, this combination can become difficult to package.

 

πŸ‘Ž Noise and Cooling Concerns

VFD-driven AC motors generate noise from motor-mounted cooling fans, drive cooling fans, and audible switching noise at certain speeds/frequencies.  In noise or temperature-sensitive environments, such as medical equipment, lab automation, or consumer-facing machinery, this can be a significant drawback.

 

πŸ‘Ž Energy Losses and Heat

Induction motors generate torque by inducing current in the rotor.  This creates rotor copper losses, which turn into heat inside the motor.  At partial load or low speeds, efficiency decreases even more.  Even inverter-duty-rated motors cannot eliminate these losses and heat.

 

πŸ‘Ž Limited Efficiency at Variable Speed

While VFDs enable speed control, AC induction motors remain most efficient at their rated operating speed.  In applications with frequent speed changes, lighter-than-rated loads, or prolonged operation at reduced speeds, excessive energy consumption can add up quickly.

 

πŸ‘Ž Lower Maximum RPM and Narrower Speed Range

VFDs and AC motors typically run only up to 2,400 RPM (80 Hz for a 4-pole AC induction motor).  BLDC motors can run up to 4,000 RPM or more.  Speed range is also wider; for example, BLDC motors can operate over a full range from 1 to 4,000 RPM, and AC motors operate from about 90 to 2,400 RPM.

 

What is a BLDC Motor?

 

 

A BLDC (Brushless DC) motor is a brushless, electronically commutated permanent magnet (PM) motor that typically uses multi-pole, 3-phase windings in its stator and permanent magnets on the surface of its rotor.  A driver is required to energize its stator phases in a controlled sequence. Typically, hall effect sensors and encoders are used to close the loop to provide the logic and speed regulation.  In other cases, the driver uses the motor's back EMF in sensorless mode. 

The controlled stator phase excitation sequence causes the rotor to follow the rotating magnetic field in the stator and rotate continuously at the commanded speed (RPM).  The commutation method can be either square-wave (trapezoidal) commutation for standard performance or sine-wave commutation (Field-Oriented Control) for more precise current control and smoother performance. 

In practice, this means a BLDC motor behaves like an AC permanent magnet synchronous motor (PMSM) but uses BLDC-style commutation.  Unlike brush DC motors, which also use permanent magnets, BLDC motors do not use brushes, so no brush maintenance is required.  BLDC motors are specifically paired with a dedicated driver for specific frame sizes, but some are also compatible with certain VFDs from other brands.

 

Tech Tip: What is a VFD, and What Types of Motors Can a VFD Drive?

A variable frequency drive (VFD) is an electronic motor drive that converts fixed-frequency, fixed-voltage AC to variable-frequency, variable-voltage AC to control the speed and torque of an AC motor.  It's most commonly used with 3-phase squirrel-cage induction motors, but it can also drive 3-phase wound-rotor induction motors, synchronous motors (ie: PMSM), and sometimes single-phase AC induction motors.  With the right architecture and operation mode, certain VFDs can also drive DC motors, such as BLDC permanent magnet (PM) motors.

⚠️ Most VFDs are set up to run in open-loop control with AC induction motors by default.  Using a VFD with a BLDC motor without changing its settings may result in poor performance or instability, so make sure you're using a VFD/inverter that can drive BLDC (PM) motors, and set it to the right control mode or motor type.  To enable feedback control, connect your feedback and switch from open-loop V/f control to motor-position-based electronic commutation.

 

How BLDC Differs from Induction Motors
A major difference between BLDC and induction motors is how the magnetic flux is generated.  Since induction motors do not use permanent magnets, the rotor's magnetic field is generated by inducing a current in the rotor.  This method is inefficient and decreases torque density, generates more heat, and increases the size of AC motors.  A slip is also created between the stator field speed and the rotor speed, which makes AC motors less synchronous than BLDC motors.


Design Differences Between a BLDC (PM) Motor and an AC Induction Motor

Feature AC Induction Motor BLDC (PM) Motor
Footprint ❌ Requires larger motor and VFD enclosure βœ… More compact system designs possible
Rotor design ❌ No magnets βœ… Uses permanent magnets
Rotor losses ❌ Copper losses present βœ… Minimal
Slip ❌ Required βœ… None (synchronous)
Torque Density ❌ Low torque density βœ… High torque density
Efficiency ❌ Low (especially at partial load) βœ… Higher  due to magnets 
Heat Generation

❌ Higher (especially at low speeds); often requires shaft-mounted fans

βœ… Lower; also fanless due to lower losses and lower operating temperature
Operating Principle ❌ Torque produced by induced rotor current (requires slip) βœ… Torque produced by permanent magnets on the rotor (synchronous)

 

How Do BLDC Motors Resolve Common Challenges of AC Motors?

   

Due to their design and characteristics, BLDC (PM) motors resolve most of the common challenges presented by AC motors.  Most noticeable is the size difference between the motors, but there are several reasons.

 

πŸ‘More Compact Systems

Because permanent magnets provide the rotor's magnetic field:

    • No rotor excitation current is required
    • Higher torque density is possible
    • Smaller motor frames can deliver equivalent torque

In many cases, engineers can reduce overall system footprint by replacing AC motors and VFDs with smaller BLDC motors and matched drives.  For example, a 1 HP BLDC motor can be 90 mm shorter and 10.2 kg lighter than a 1 HP AC motor.  In many cases, the BLDC driver can also be smaller.

 

πŸ‘Lower Noise

BLDC motors typically:

    • Run cooler due to reduced losses
    • Do not require built-in cooling fans
    • Can be designed without external cooling fans

With approximately 20 dB reduction, this makes BLDC motors especially attractive for quiet environments and applications where airflow is undesirable (ie: medical, food processing, or clean rooms). 

 

πŸ‘Higher Energy Efficiency

With no rotor copper losses:

    • Electrical efficiency improves
    • Less heat is generated
    • Performance remains consistent at variable speed and partial load

For systems that run many hours per day or operate under energy constraints, the efficiency gain alone can justify considering a BLDC motor.  Replacing an AC motor with a BLDC motor can result in a decrease of $89/year per motor.

 

πŸ‘Better Control at Low Speed

Electronic commutation enables:

    • Precise speed regulation
    • Fast acceleration and deceleration
    • Strong low-speed torque without slip

Many VFDs cannot run AC motors below 90 RPM while BLDC motors have no problems operating close to 0 RPM.  This is especially useful in indexing, positioning, and variable-speed automation tasks where slow speeds are required.

 

πŸ‘Keep Your VFD

With the right architecture, certain VFDs can be set up to run BLDC (PM) motors.  This means:

    • Upgrade your motor quickly without changing your preferred controls
    • Flat torque characteristics and wider speed range
    • Lower power consumption and motor temperature

Many BLDC motor manufacturers offer their own BLDC drivers.  If the existing VFD is preferred, there's an option to upgrade just the motors.  The key is selecting a VFD that's also compatible with BLDC (PM) motors.  For help with compatibility or settings, please contact the manufacturer of the motor or the VFD.

 

This video compares a 1 HP AC induction motor with a 1 HP BLDC motor.

 

Performance Differences Between a BLDC (PM) Motor and an AC Induction Motor

Category AC Induction Motor with VFD BLDC (PM) Motor with VFD

Upfront Cost

βœ… Lower motor and drive cost ❌ Higher motor + dedicated drive cost

Efficiency (Rated Load)

❌Good at or near rated speed and load βœ… Very high at rated conditions

Efficiency (Partial Load)

❌ Drops significantly at reduced speed or light load βœ… Maintains high efficiency across wide speed range

Torque Density (Size/Output)

❌ Larger frame for same torque βœ… Higher torque density β†’ smaller, lighter motors

Noise

❌ Fan noise and PWM‑related acoustic noise possible βœ… Generally quieter; smoother torque

Vibration

❌ Can increase at variable speed or low frequency βœ… Typically smoother, especially at low speed

Variable Speed Control

❌ Good, but frequency‑based; low‑speed control depends on tuning βœ… Very fine speed and torque control via electronic commutation

Low-Speed Torque

❌ Limited without advanced vector control βœ… Strong low‑speed torque without slip

 

When to Choose BLDC vs. Induction Motors

The decision ultimately depends on your application priorities. Here's a practical breakdown.

 

βœ… Choose BLDC Motors When:

βœ… Choose Induction Motors When:

πŸ‘ High efficiency is needed at variable speeds or partial loads

πŸ‘ Space is constrained and high torque density is valuable

πŸ‘ The application requires precise speed or torque control

πŸ‘ The system is battery-powered or energy-limited

πŸ‘ You want low noise, reduced heat, and low maintenance

πŸ‘ Lowest upfront cost is the main constraint

πŸ‘ The system runs mostly at constant speed

πŸ‘ You need a rugged and industrial solution

πŸ‘ Efficiency at light load is not critical

πŸ‘ Control precision requirements are minimal

 

Besides the obvious AC vs DC power supply difference, AC induction motors and BLDC motors can be used for the same applications, such as conveyors and pumps.  The difference is that these conveyors and pumps can be made smaller, less noisy, and more efficient with BLDC motors.

Instead of selecting based on specifications alone, take a system-level approach and compare motor options against your actual load curve, duty cycle, and drive requirements.  An induction motor can still be practical and cost-effective for many industrial applications, but a BLDC motor delivers long-term energy savings and performance gains that eventually overcome the initial upfront costs.

If you're designing a new system or upgrading an existing one, aligning motor choice with real operating conditions (not just peak specs) will ensure optimal performance and ROI.

 

Recommended Product

Oriental Motor's BLDC Motors for Inverters are compatible with 3rd-party inverters in the market and offer a lineup from 120 W (1/6 HP) to 750 W (1 HP).  Performance datasheets are provided for popular VFDs.

These BLDC (PM) motors are compatible with:

βœ… ABB ACS380

βœ… Fuji Electric FRENIC-Mini

βœ… Innovance MD600

βœ… Lenze i550

βœ… Mitsubishi Electric D-800 or E-800

βœ… Rockwell Automation Allen Bradley PowerFlex525

βœ… Schneider Electric Altivar Machine ATV320

βœ… Siemens G120

βœ… Toshiba VF-S15

Performance datasheets are provided online.

Need a higher IP rating?  We also offer an IP69K rated stainless steel 200 W (1/4 HP) BLDC gear motor (part of BLE2 Series).

 

Related articles:

 Head-to-Head: 1 HP BLDC Motor vs 1 HP AC Induction Motor 

 VFD vs BLDC: Which Technology is Better for Speed Control? 

 Brush DC Motors vs Brushless DC Motors: Which is Better? 

 

Topics: AC Motors, Speed Control, BLDC Motors

Johann Tang

Written by Johann Tang

Johann Tang is a Product Specialist at Oriental Motor USA Corp. Before joining the marketing team, he spent 14 years in sales and technical application support, and he also led product training on various types of fractional-horsepower electric motors, gear motors, actuators, drivers, and controllers. If you have any questions, please feel free to use the live chat window, 1-800-GO-VEXTA (1-800-468-3982), or techsupport@orientalmotor.com, to reach our product support team. Sorry, comments have been turned off.

    Subscribe Here!

    Recent Posts

    New call-to-action