Engineering Notes by Oriental Motor

Improve BLDC Motor Performance With Updated Drivers

[fa icon="calendar"] Originally posted on Feb 23, 2026 6:59:14 PM
Last updated on February 24, 2026 / by Johann Tang

Johann Tang

Improve BLDC Motor Performance With Updated Drivers
12:32

At Oriental Motor, continuous improvements are part of our process.  This article takes a deep look at functional updates of our popular BLH Series drivers, how they differentiate from existing drivers, and how they can improve functionality and performance.

Newly redesigned BLH series brushless motor drivers

 

The BLH Series BLDC (brushless DC) motors and drivers have been popular for a long time, and there is a good reason why. Our customers seem to favor the combination of an efficient, compact gear motor and a small, easy-to-use driver.

Over the years, we listened to our customers and heard the need to improve driver functionality, including the ability to digitally set speeds rather than rely on analog signals, the need to communicate with host controllers, and the preference for better performance and updated technologies.

The result? We released three new types of drivers: Analog Setting Type, Digital Setting Type, and RS-485 Communication Type.

From RS-485 communication capability to vector drive technology, the improvements don't stop at the driver but also enhance motor performance. Let me tell you what's really different about these updated BLH Series drivers.

 

What's Covered?

  • Adopting Vector Control
  • Improvements in Performance
  • Benefits of the Digital Setting Type and RS-485 Communication Type Drivers
  • Analog Setting Type vs Digital Setting Type vs RS-485 Communication Type
  • Summary

 

Adopting Vector Control

✅Vector Control

All 3 updated BLH Series drivers introduced a major leap in performance with Vector Control for brushless DC motors (AKA "FOC" - Field Oriented Control), delivering smoother motion, more torque, and higher efficiency than older drive technologies.  By precisely controlling the current phase and generating a sinusoidal current waveform, the updated drivers unlock features like regenerative power handling and reliable torque limiting.   Even with standard Hall Effect sensors, these updated drivers can intelligently interpolate rotor position to achieve full vector‑control precision.

 

vector control for BLH series BLDC motors Interpolation of Position Information

 

Better current control leads to many benefits like increased torque and lower noise.  In addition, we also improved driver functions like software compatibility, stored data capability, and fieldbus communication.  Let me go over these updated features.

 

Improvements in Performance

✅Increased Torque

Although there is no design change to the motors, when these updated BLH Series drivers are used with existing BLH Series motors, torque performance improves in both the limited-duty and continuous-duty regions.  The increased torque can be used to move more load, or accelerate/decelerate faster.

 

BLH brushless motor redesign: increased torque

 

✅Extended Acceleration/Deceleration Range & 3 Stop Modes

With the updated drivers, the acceleration/deceleration time setting range has been extended both in the low end and high end.  In addtion, 3 "deceleration stop" modes are provided for more flexibility in stopping the motor.

 

Type of BLH Series Driver Acceleration/Deceleration Range
Older Drivers (Analog Only) 0.5~10 seconds
New Analog Setting Type Drivers 0.1~12 seconds
New Digital Setting Type Drivers 0.1~15 seconds
Stop Mode Description

Deceleration Stop 1

deceleration stop type 1 timing chart

The motor generates a braking force when decelerating to a stop, and operates so as to stop according to the set deceleration time setting.  Regenerative power generated by the deceleration of the motor, it is consumed by the motor and driver and won't return to the power supply side.

Deceleration Stop 2

deceleration stop type 2 timing chart

The motor coasts to a stop by suppressing a braking force at deceleration stop.  However, if the deceleration time is shorter than the time that the motor takes to coast to a stop, it will not be applied.

Deceleration Stop 3

deceleration stop type 3 timing chart

The motor generates a braking force when decelerating to a stop, and operates so as to stop according to the set deceleration time.  The regenerative power generated by the deceleration of the motor is returned to the power supply side.

 

Why do we offer 3 different ways to decelerate? 

For example, in applications such as driving mechanisms for AGVs and AMRs, back EMF generated by back-driving of motors is a major issue.  Using Deceleration Stop 1 could help eliminate power supply and driver issues due to back EMF.  Using Deceleration Stop 3 could recharge the battery for the vehicle.  Just make sure the battery can absorb the regenerative power.

 

BLH brushless motor with hollow shaft gearhead for AGVs

 

✅Lower Noise

Another nice improvement of the updated BLH Series drivers is lower overall noise due to improved current waveform control.  With reduced torque ripple and smooth rotation even at low speeds, the motor's drive noise is reduced by 13 dB

Watch the video below to get an idea of the difference in noise.

 

 

 

Now I'll go over the differences between the 3 types of drivers.

 

Benefits of the Digital Setting Type and RS-485 Communication Type Drivers

The older BLH Series drivers with square-wave drive technology were the original Analog Setting Type. Analog Setting Type drivers allow the speed(s) to be set by an analog voltage signal. This signal can be provided by an internal potentiometer, an external potentiometer, or a 0~5VDC external signal.

The problem with analog signals is their tendency to vary due to cable resistance changes.

The Digital Setting Type driver includes more features and functions to improve the overall performance and ease of use. Along with adding vector drive technology, compatibility with our MEXE02 universal data setting software is also introduced for easier digital setting of data and better troubleshooting. I'll explain more later.

To meet predictive maintenance requirements or reduce wiring requirements, an RS-485 Communication Type driver is available. Two communication ports are added as well as MEXE02 support software compatibility. Once connected to a upper level host controller, this driver will be able to send real-time updates on various status data. Specifications such as speed regulation and speed range will be the same as the Digital Setting Type driver.

 

Digital Setting Type RS-485 Communication Type
BLH Series digital setting type BLDC motor driver BLH Series RS-485 communication type BLDC motor driver

The Digital Setting Type and RS-485 Communication Type drivers are not offered for 100 W motors at this time.

 

✅MEXE02 Support Software

For both the Digital Setting Type and RS-485 Communication Type drivers, one major design change was adding a USB connector on the driver board and compatibility with the MEXE02 support software (our universal GUI motion data programming software). Many of the new features and functions are possible because of this software.

 

MEXE02 motion programming software

 

One advantage is obviously the ability to set motion data and parameters by digitally setting them instead of flipping tiny dip switches or relying on analog signals, but there are many more.

 

✅Better Speed Regulation, More Data Sets, and Wider Speed Range

Since we are now "digitally" setting the data, the speed regulation is improved from +/-0.5% to +/-0.2%. This means that the motor will only have a maximum error of +/-0.2% even with changes to load. This enhanced speed regulation can help improve synchronous operations with multiple motors.

 

Speed regulation comparison between BLDC drivers 

With the MEXE02 software, 8 speed data sets can be programmed and set within the stored data bank of the driver. With the older analog setting drivers, only 2 speeds can be set by a potentiometer or an analog DC voltage.

With digital speed setting, the speed range is also widened a little bit on the low end (100~3,000 RPM vs 80~3,000 RPM), which opens up the BLH Series for more low speed applications.

 

✅I/O Function Selection

MEXE02 SW: I/O function selection

With the MEXE02 software I/O function selection, the user can assign the input function they need instead of something that's not necessary for the application.

Even though you have 6 inputs and 4 outputs physically available, there are more functions you can assign based on your preference.

 

✅Torque Limiting

Torque limiting is a function to limit the motor's torque to a percentage of the rated torque (100%) by using current and feedback.

Torque limiting function

For applications such as pressure-sensitive stamping, pressing, capping or screwing operations, a built-in torque limit function can be very useful. Torque limiting application example: capping

 

✅PWM Input (Digital Setting Type)

The Digital Setting Type driver can also accept a PWM signal from the PLC to set speed instead of using an external DC voltage. This could help eliminate the extra cost of an analog card on the PLC.

PWM input on BLH Series BLDC motor driver

 

✅Teaching Operation and Data Copy Function

The teaching operation allows speeds to be taught by the software's speed toggle function.

For data synchronization between multiple drivers, a data copy function is available.

MEXE02 SW: teaching/remote operation, operating data copy and reading

 

✅Remote Monitoring and Predictive Maintenance

Remote monitoring allows monitoring of system status in real time through the MEXE02 software. Through this function, data such as speed, load factor, driver temperature, load, tripmeter, odometer, I/O status, alarm codes, and power cycles can be monitored by the software. For predictive maintenance, information bit outputs can be easily configured and sent to the PLC by RS-485 communication standard and Modbus (RTU) protocol.

 

MEXE02 SW: status monitoring, information monitoring, and alarm monitoring

 

Related Post: Introduction to MEXE02 Support Software for Stored Data Type Drivers (VIDEO)

 

Analog Setting Type vs Digital Setting Type vs RS-485 Communication Type

The following table compares the features of the 3 types of BLH Series drivers we offer.

 

Driver Type

Analog Setting Type

Digital Setting Type

RS-485 Communication Type

 

BLH Series analog setting type BLDC motor driver

BLH Series digital setting type BLDC motor driver

BLH Series RS-485 communication type BLDC motor driver

Features

Simple speed setting by volume or external analog signal

Start/stop control via I/O

Setting from PC using support software MEXE02

Start/stop control via I/O

Configuration via network using Modbus communication

Direct control of operation and shutdown from the host

Output

15W/30W/50W/100W

15W/30W/50W

15W/30W/50W

Speed ​​Control Range

100 to 3000 rpm

80 to 3000 rpm

80 to 3000 rpm

Speed ​​Setting Method

Internal speed potentiometer

-

External speed potentiometer

External DC Voltage

PWM signal

-

MEXE02

-

MEXE02 Software
MEXE02 Software

RS-485 communication

-

-

Function

Instantaneous stop

Acceleration and deceleration operation

Multi-speed operation

Synchronized Operation

Load factor display

-

Torque Limit

-

Load Holding Function

-

Deceleration to a stop

-

Information

-

 

TIP Connector Location Change

When switching from the Analog Setting Type driver to the Digital Setting Type Driver, notice that for the new drivers, the motor connector is now on the left side instead of right side. There's a USB connector on the digital setting type drivers. Please use a USB2.0 cable to connect to your PC after installing the MEXE02 software.

Older BLH Series Driver Updated BLH Series Drivers
Analog Setting Type Analog Setting Type Digital Setting Type
BLH Series analog setting type BLDC motor driver (old) BLH Series analog setting type BLDC motor driver (updated) BLH Series digital setting type BLDC motor driver

①Power Connector

②I/O Signal Connector

③Motor Connector

④USB Connector (for digital setting type)

 

Summary

The updated BLH Series compact BLDC drivers deliver higher torque, faster acceleration and deceleration, and greater stopping flexibility, all without changing the motors themselves. Users gain improved performance through extended accel/decel ranges, three new regenerative‑friendly stop modes, and the option to choose analog, digital, or RS‑485 driver types. These enhancements help reduce tact time, improve control, and solve issues like back‑EMF in applications such as AGVs and AMRs—making the updated drivers more powerful, more flexible, and easier to integrate.

 

TIP Make sure to use BLH Series drivers with part numbers starting with "BLH2D" for the updated drivers with vector drive technology. FYI part numbers for the older drivers begin with just "BLHD".

 

 Demo  Watch the BLH Series drive an AGV

BLH Series

Download Brochure

 

For brushless motors higher than 1/8 HP  (100 W) combined with DC input drivers, we recommend the BLV Series R Type.  For help finding the most suitable product for your specific application, please contact our technical support team.

 

Topics: Torque Limit (Push Motion, Tension Control), Robotics, Speed Control, VIDEOS, BLDC Motors, Software, Bottle Capping, AGV/AMR

Johann Tang

Written by Johann Tang

Johann Tang is a Product Specialist at Oriental Motor USA Corp. Before joining the marketing team, he spent 15 years in sales, technical application support, and training of various types of fractional horsepower electric motors, gear motors, actuators, drivers, and controllers. If you have any questions, please feel free to use the live chat window, 1-800-GO-VEXTA (1-800-468-3982), or techsupport@orientalmotor.com, to reach our product support team. Johann can be reached via LinkedIn. Sorry, comments have been turned off.

    Subscribe Here!

    Recent Posts

    New call-to-action