Engineering Notes by Oriental Motor

Introduction to the OVR Series Small Industrial Robots

[fa icon="calendar"] Dec 11, 2024 12:00:11 PM / by Johann Tang

Johann Tang

Introduction to the OVR Series Small Industrial Robots
12:36

Learn more about Oriental Motor's compact and easy-to-use small industrial robots, robot controllers, and software.

Topics Covered:

  • Hit the Easy Button
  • What Types of Robots are Included in the OVR Series?
  • Robot Control and Programming
  • Try Out Our New Test Tools
  • OVR Series Robots in Action

Building a robot is not easy.  It involves designing, selecting, assembling, integrating, programming, and testing various components and making sure they work in synchronization with other axes to perform specific tasks.  It is much easier said than done.  There are also many mechanical, control, precision, and safety parameters to consider:

Mechanical Considerations:

  • Must be rigid for precision but light for speed
  • Complex joint design with minimal backlash
  • Thermal expansion affects accuracy

Control Considerations:

  • Real-time processing (millisecond responses)
  • Complex mathematics for movement: p=f(θ1,θ2,...,θn)p = f(θ_1, θ_2, ..., θ_n) (coordinate transformation)
  • Must account for inertia, gravity, friction

Precision Considerations:

  • Repeatability (±0.01mm typically)
  • Maintain accuracy under varying loads/speeds
  • Requires high-quality sensors and feedback

Safety Considerations:

  • Emergency stops, collision detection
  • Speed/force limits
  • ISO compliance

All selected components, such as motors, gearheads, actuators, drivers, and even couplings, must meet the required specifications.  Each type of robot also has its own unique challenges.  For example, SCARA needs selective compliance, Cartesian needs precise linear motion, and articulated robots need complex joint coordination.  For basic information on how to build an articulated robot, please refer to this article: How Easy Is It to Build a Robot?

Is there an even easier way?

 

Hit the Easy Button  Staples Talking That Was Easy Button Complete With Batteries - 1 each

More often than not, it's easier to buy a robot.  To help engineering teams that don't necessarily have the resources or team size to build robots but are interested in robotic automation, Oriental Motor has released a line of easy-to-use compact industrial robots designed to transfer small parts.  

 

 

 

Customers can select from a 4, 5, or 6-axis Vertically Articulated robot, a 3-axis SCARA robot, or a 3-axis Cartesian robot and combine it with an end-effector, such as our 2 or 3-finger gripper.

All the moving axes utilize motors, linear/rotary actuators, and mini drivers from the AlphaSTEP AZ Series Hybrid Step-Servo Product Family.  With its patented mechanical absolute encoder technology, absolute position control can be achieved without a backup battery, such as in the case of an optical absolute encoder. αSTEP Mechanical Absolute Encoder

To help simplify the programming of these types of robots, we have also released new MRCU Integrated Robot Controllers, which combine the powerful MRC01 Robot Controller and up to 7 AZ Series mini drivers in a small box.   The drivers, cables, and the Robot Controller are pre-assembled, which means that all users have to do is connect the motors, actuators, or grippers.

 

What Types of Robots are Included in the OVR Series?

The OVR Series lineup includes 3 types of compact industrial robots that can provide a cost-effective alternative to similar industrial robots in the market.  The entire robot, as well as its drivers and controllers, can be powered by a single DC power supply, which means that these robots can easily be mobile as well.  By using modular, standard components instead of custom components, these small robots can help reduce costs, shorten lead times, and simplify maintenance.

 

 New  Articulated Robot   New  SCARA Robot  New  Cartesian Robot
ovr4068k5-v-img-200px
ovr3041k3-h-img-200px
ovr3ar030030z10k-c-img-200px
  • 4, 5, or 6 axis
  • Compact and lightweight
  • Can be combined with an electric linear slide for horizontal travel (5/6-axis)
  • Transportable mass: 1~5 kg
  • 3-axis
  • Fits in tighter spaces 
  • Lightweight and flat, low-profile design (7.6 kg and 140 mm height)
  • Transportable mass: 3 kg
  • 3-axis
  • 3 linear slides pre-assembled
  • Moving range 300 mm × 300 mm × 100 mm (X-Y-Z)
  • Transportable mass: 2.5 kg

 

For the end-effector (wrist rotation) on the vertically articulated robots, a Robot Flange Adapter that conforms to ISO 9409-1-31.5-4-M5 standard is available to mount our EH Series compact gripper.  If another manufacturer's end-effector is preferred, adapter plates can be purchased from other manufacturers.  For the SCARA and cartesian robots, a custom adapter plate can be made.

 

Robot Flange Adapter

 

Vertically Articulated Robots

Application: capable of approaching and picking parts from multiple directions.

The vertically articulated robots are our best sellers in Japan and offer the highest payload in the OVR Series.  There are 3 models available with different movable ranges.  The arms can be replaced by different lengths for some customization. The 6-axis articulated robot offers the maximum degree of freedom and can approach the load from different angles.

 

# of Axes 4-Axis 5-Axis 6-Axis  
Design 4-axis Small OVR Robot OVR5035K1-V Small Articulated OVR Robot 6-axis Small Articulated OVR Robot  
Feature

Parallel link mechanism

Compact and lightweight

Approach the load from various angles

 
Maximum Reach (Horizontal)

480/680/880 mm

350 mm

480 mm

 
Transportable Mass 5 kg 1 kg 1 kg  

 

This system configuration example shows how the robot can be connected to the MRCU Series Integrated Robot Controller and other existing equipment, such as a PLC/IPC.

 

 

Here's what a 6-axis vertically articulated robot looks like.  We also break down its motion axes and control components.

 

Components of a 6-Axis Vertically Articulated Robot

Robot Model: OVR6048K1-V

Axis 1: DGII Series Hollow Rotary Actuator

Axis 2~5: AZ Series Hybrid Step-Servo Motors

Axis 7?  Connect your own end-effector

(Shown: EH Series 3-Finger Type Compact Gripper)

Integrated Robot Controller: MRCU6A1D*

*Contains MRC01 Robot Controller (1 pc) + AZD-KR2D mini Drivers (6 pcs)

MRCU Integrated Controller & Drivers

 

Various end-effectors can be used to pick up parts at the end of the arm (7th axis), including our 2 and 3-finger type EH Series compact grippers.  For light loads (up to 5 kg), these articulated robots can serve as cost-effective alternatives to other small robots in the market.  The 5-axis and 6-axis articulated robots can also be combined with an electric linear actuator or a mobile robot to meet linear travel or mobile requirements.

 

Horizontally Articulated (SCARA) Robots

Application: capable of moving parts in and out of narrow spaces.

The OVR Series horizontally articulated robot (SCARA) is offered in a 3-axis configuration.  The space-saving, low-profile design of the SCARA robot makes it possible to move parts in and out of tight and narrow spaces.  A DGII Series Hollow Rotary Actuator is used at the base of the SCARA robot to handle handle high moment loads.

 

# of Axes 3-Axis
Design 3-axis SCARA OVR Robot
Feature

Low-profile design

Maximum Reach (Horizontal)

410 mm

Transportable Mass 3 kg

 

The vertical height of the OVR Series SCARA robot is only 137 mm.

 

 

This system configuration example shows how the robot can be connected to the MRCU Series Integrated Robot Controller and other existing equipment, such as a PLC/IPC.

 

3-axis SCARA MRCU System Configuration

Components of a 3-Axis SCARA Robot

Robot Model: OVR3041K3-H

Axis 1: DGII Series Hollow Rotary Actuator

Axis 2: AZ Series Hybrid Step-Servo Motors

Axis 3:  DGII Series Hollow Rotary Actuator

Axis 4?  Connect your end-effector

(Shown: EH Series 2-Finger Type Compact Gripper)

3-Axis Integrated Robot Controller: MRCU3A1D*

*Contains MRC01 Robot Controller (1 pc) + AZD-KR2D mini Drivers (3 pcs)

MRCU Integrated Controller & Drivers

 

Various end-effectors can be used to pick up parts at the end of the arm (4th axis), including our 2 and 3-finger type EH Series compact grippers.  If you need a low-profile SCARA robot to pick up small parts in a narrow space, this robot can be your answer.  This SCARA robot can also be combined with an electric linear actuator or a mobile robot to meet linear travel or mobile requirements.

 

Cartesian Robots

Application: approaching and moving parts in fixed cartesian XYZ coordinates.

This cartesian robot is delivered pre-assembled with 3 linear slides.  This is also the only type of robot that uses the MRC01-C Cartesian Robot Controller, which is a simplified version of the MRC01 Robot Controller.  The MRC01 will also work, but the simpler MRC01-C is offered at a lower price point.

 

Type L Type R Type  
Design  
Feature

Easy to control

 
Maximum Reach (Horizontal)

300 (X) x 300 (Y) x 100 mm (Z)

 
Transportable Mass 2.5 kg  

 

This system configuration example shows how the robot can be connected to the MRC01 Robot Controller, the AZD-KR2D mini drivers, and other existing equipment, such as a PLC/IPC.

 

3-axis Cartesian Right Type MRC01-C System Configuration

 

Components of a 3-Axis Cartesian Robot

Robot Model: OVR3AR030030Z10K-C

Axis 1~3: EZS Series Motorized Slide Actuators

Axis 4?  Connect your own end-effector

(Shown: EH Series 2-Finger Type Compact Gripper)

Cartesian Robot Controller: MRC01-C (1 pc) AZ Series mini Drivers: AZD-KR2D (3 pcs)

 

On the vertical Z-axis, various end-effectors can be installed on the moving table to pick up parts, including our 2 and 3-finger type EH Series compact grippers.  The 5-axis and 6-axis articulated robots can also be combined with an electric linear actuator for linear travel.

 

Robot Control and Programming

With the MRC01 Robot Controller and MRC Studio software, up to 7 axes of SCARA, cartesian, and articulated robot motion axes can be easily programmed even without prior programming experience.  An MRC01 Robot Controller can be configured for 59 different types of robots and store up to 64 programs with 128 commands each.  

  • Motion Commands: Point-to-Point, Linear, Circle (with helical interpolation), Arch
  • Control Commands: Stand by (Time), Stand by (Signal), Loop, and Signal output 

In addition, the MRC01 Robot Controller can communicate with the host controller (PLC/IPC) via EtherNetIP for data setting or monitoring.

 

Robot Controller

 

An MRCU Series Robot Controller combines an MRC01 Robot Controller with AZ Series DC-input mini drivers in a compact box, so all you have to do is connect the cables externally.

 

 New  MRCU Multi-Axis Robot Controller
mrcu-lm-feature-single-package
Rear View of MRCU Integrated Controller & Drivers

 

With its intuitive interface, the MRC Studio programming software can be downloaded to program these small robots.  No programming experience is necessary to use the software.

 

Easy Setup

Just select the type of OVR Series robot to begin setting up the stored data inside the Robot Controller. 

In addition, the MRC01 Robot Controller or any MRCU Series Integrated Robot Controller can communicate to a host controller via EtherNetIP for data setting, I/O commands, or monitoring.

Easy Setup, Even for Beginners

  

Drag and drop commands, no ladder logic

No Ladder Logic

Just drag and drop the required commands, including target positions and speed settings.  No ladder logic experience (or any programming experience) is necessary.

 

Try Out Our New Test Tools

MRC Simulator Software

A trial version of the software can be downloaded for testing.

MRC Reality (Augmented Reality)

Use the AR/MR robot function to visualize, simulate, or teach.

 

OVR Series Robots in Action

Oriental Motor not only builds robots, but we also use them to increase production efficiency and reduce errors in our own production lines.

SCARA Robot in Sensor Assembly Line  Articulated Robot Applying Grease to Ball Screws

 

Robots are a significant investment.  According to Perplexity, the price of a 6-axis vertically articulated robot capable of handling parts up to 5 kg in the United States can range from as low as $15,000 to $25,000 or more, depending on what the price includes.  The end-effector, controllers, cables, safety devices, advanced features, integration, programming, support, and training can all add to the cost.  The OVR Series small industrial robots can provide alternatives for users looking for options other than those provided by bigger brands.

As always, you can contact an Oriental Motor sales engineer or technical support engineer for a full product introduction or to answer any questions.

 

Topics: Stepper Motors, Robotics, Absolute Positioning, Alphastep Hybrid Control, Linear Actuators, VIDEOS, Software, Application Examples, New Product Introductions, XYZ/Cartesian/Gantry

Johann Tang

Written by Johann Tang

Johann Tang is a Product Specialist at Oriental Motor USA Corp. Before joining the marketing team, he spent 15 years in sales, technical application support, and training of various types of fractional horsepower electric motors, gear motors, actuators, drivers, and controllers. If you have any questions, please feel free to use the live chat window, 1-800-GO-VEXTA (1-800-468-3982), or techsupport@orientalmotor.com, to reach our product support team. Johann can be reached via LinkedIn. Sorry, comments have been turned off.

    Subscribe Here!

    Recent Posts

    New call-to-action
    Product Guide