Engineering Notes by Oriental Motor

Wrap Function: Simplified Position Control for Rotary Indexing in Absolute Coordinates

[fa icon="calendar"] Originally posted on Jan 4, 2019 7:56:17 PM
Last updated on April 13, 2023 / by Johann Tang

Johann Tang

With recent trends focusing on improving engineering efficiency, many products have been developed to specifically help shorten design cycles for machine automation.  Part of improving efficiency is making products easier to use, so additional time and resources can be spent elsewhere.  This post describes a product feature that can make index table applications less complex to manage.

Rotary index table

APPLICATION EXAMPLE: rotary index table that rotates a fixed distance repeatedly in the same direction.  A motorized rotary actuator is installed below the index table. 

The product video below shows a similar application example of a syringe dispensing application; also with a rotary actuator.

For an index table that rotates a fixed distance repeatedly in the same direction, position management can be difficult since the internal position counter value keeps increasing.  Some mathematical calculations are necessary to convert the step count to degrees before the operator can understand where the table is actually facing.

 

For example, let's say we are positioning 90 degrees at a time with a motor that has a basic step resolution of 200 steps per revolution, or 1.8° per step.  The position counter value will look like this:

Steps 0 50 100 150 200 250 300 350 400 450 500
Degrees 90° 180° 270° 360° 450° 540° 630° 720° 810° 900°

 

On a rotary table, the same index positions repeat after 360 degrees, the actual position coordinates within 360° have to be calculated.

 

Here's a simple formula to figure out the actual position coordinates. 

Actual Position = Current position in degrees - (360 x number of revolutions travelled)

For 900°, the rotary table has rotated more than 2 revolutions, so the formula will be:

Actual Position = 900° - (360° x 2) = 180° (from home position)

 

Is there an easier way to do this?

 

Challenge
Manage 360° coordinates better by converting to absolute coordinates instead of steps

For positioning management of index tables, it is easier to monitor the table position if the position count value can be set in degrees as well as clear the position counter once it passes 360°.  For the above example, the position values can be converted from step count to degrees, which makes life just a little easier.  Other functions, such as Wrap Proximity Positioning and Wrap Absolute Positioning, can be used to make position control and management even easier.

 

Solution
Use the Wrap Function to reset position counter when appropriate

The Wrap Function automatically resets the position counter value to 0 when the motor output shaft exceeds a set value.  For example, when the "Wrap Setting Range" is set to "1 rotation", the position counter value automatically resets to 0 when the motor shaft exceeds 360° from the home position.  Gear ratios can also be added to additional adjustments.

Wrap function setting flow chart

Here we show you a screenshot of the dedicated MEXE02 support software where it contains the Wrap parameter settings.

Left Menu:

MEXE02 wrap menu

Center Window:

Wrap function setting-1

The circled parameters are changed from their default values to make this possible.

Initial Coordinate Generation & Wrap Coordinate Setting

To use the wrap function, select manual
setting.

Setting range: ABZO sensor or manual

Initial Coordinate Generation & Wrap Setting Range (rev)

Sets the wrap range. The command position
returns to 0 when the motor has rotated for
the number of times set here.

Setting range: 5 to 655,360 (1=0.1 rev)

Initial Coordinate Generation & Wrap Range Offset Ratio (%) Set the offset ratio of the wrap range.
Setting range:  0 to 10,000 (1=0.01%)
Wrap Setting Enable or disable
The Number of the RND-ZERO output in wrap range

Sets the number of times to turn the
RND-ZERO output ON in the wrap
range.

Setting range: 1 to 536,870,911 divisions

 

Here's a video showing you how to set up the Wrap Function parameters for Oriental Motor's rotary actuators by using the MEXE02 support software.

 

  Bonus: Learn the various types of Wrap positioning operations you can do with this video tutorial.

 

For more information about the Wrap Function, please refer to page 40 of the AZ Series Functions Manual.* 
*The DG II Series is the hollow rotary actuator version of the AZ Series.


Product Highlight: DG II Series Rotary Actuators

  • Low profile
  • AC and DC versions available
  • 60/85/130/200 mm frame sizes
  • Built-in absolute position sensor
  • Permissible torque up to 50 Nm (440 lb-in)
  • Moment load up to 100 Nm (880 lb-in)
  • Thrust load up to 900 lbs (408 kg)
DG II Series hollow rotary actuators
Learn More Watch More Videos

 

The Wrap Function is available with products from the AlphaStep AZ Series Family  , such as EZS linear slides, EAC linear cylinders, DGII Series rotary tables, DRS/DR compact cylinders, L rack and pinion systems, and EH gripper systems.  

 

Interested in learning more about the AlphaStep family?

Schedule a Demo  

 

Topics: Stepper Motors, Absolute Positioning, Linear Actuators, VIDEOS, Software, Application Examples

Johann Tang

Written by Johann Tang

Johann Tang is a Product Specialist at Oriental Motor USA Corp. Before joining the marketing team, he spent 14 years in sales and technical application support, and he also led product training on various types of fractional-horsepower electric motors, gear motors, actuators, drivers, and controllers. If you have any questions, please feel free to use the live chat window, 1-800-GO-VEXTA (1-800-468-3982), or techsupport@orientalmotor.com, to reach our product support team. Sorry, comments have been turned off.

    Subscribe Here!

    Recent Posts

    New call-to-action