Engineering Notes by Oriental Motor

Coordinated Robots Bring Precision and Flexibility to Automated Bottle Capping

[fa icon="calendar"] Originally posted on Apr 27, 2026, 8:00:00 PM
Last updated on June 25, 2026 / by Johann Tang

Johann Tang

Coordinated Robots Bring Precision and Flexibility to Automated Bottle Capping
8:50

As packaging lines face increasing pressure to run faster, handle more variants, and fit into tighter footprints, automation strategies must balance precision, flexibility, and size. One effective approach is the coordinated use of compact robots integrated with machine vision - an architecture well-suited for highly repeatable tasks like bottle handling and capping.

What's covered?

  • Introduction
  • Step 1: Bottle Handling with a Low‑Profile SCARA
  • Step 2: Identify Variability with Machine Vision
  • Step 3: Bottle Cap Pick-and-Place with Vision-Integrated Articulated Robot
  • Summary & Design Tips

 

Introduction

The demo video shows an OVR Series 4-axis articulated robot and an OVR Series 3-axis SCARA working in tandem to unpack bottles, identify caps using a camera, perform accurate capping, and repack the finished product.  This demonstration illustrates how a system design that combines the right robot form factor, integrated vision, and coordinated motion can deliver reliable, high-precision packaging automation even in space-constrained environments.  The result is a compact, highly synchronized automation cell designed for consistent throughput and easy scalability.

 

Bill of Materials:

1 pc OVR Series 3-axis SCARA [ OVR3041K3-H ]

1 pc OVR Series 4-axis articulated robot  [ OVR4068K5-V ] 

1 pc EH Series 2-Finger Electric Gripper [ EH4-AZAKH ] (with PDG60-2 gripper mounting bracket)

1 pc OnRobot Electric Gripper [ 2FG7 ] (mounted directly to ISO 9409-1-31.5-M5 flange)

2 pcs MRCU Series 4-Axis Integrated Robot Controller (includes dedicated drivers) [ MRCU4AK ]

1 pc Cognex In-Sight 2800 vision camera

1 pc Rockwell Automation Allen Bradley CompactLogix 1769 Programmable Logic Controller

 

Compatible with 3rd Party Devices

 With easy mounting options and direct EtherNet/IP and RS-485 communication, the OVR Series robots can be easily integrated with devices from other companies, such as an end-effector and a vision camera.  Our EH Series 2-finger electric gripper is mounted at the end of the OVR Series 3-axis SCARA arm using a PDG60-2 mounting bracket, while a 3rd-party electric gripper from OnRobot is mounted to the ISO 9409-1-31.5-M5 standard mounting flange on the arm of the OVR Series 4-axis articulated robot.  The dedicated MRCU Series robot controller for the 3-axis SCARA communicates with its EH Series gripper, and the dedicated MRCU Series robot controller for the 4-axis articulated robot communicates with its OnRobot gripper. 

 

Step 1 Bottle Handling with a Low‑Profile SCARA

The process begins with the OVR Series 3-Axis SCARA Robot (Bottle Handing Robot) on the right side.  It's responsible for unpacking and positioning the white plastic bottles in preparation for the bottle capping process, which is performed by the articulated robot on the left.

What sets the OVR Series 3-axis SCARA Robot apart is its ultra‑low profile, measuring under 6 inches in height.  In modern packaging environments where conveyors, guards, and tooling are stacked tightly, vertical clearance is often the limiting factor. Traditional SCARA robots can struggle to reach into cartons or tightly enclosed packaging areas without additional mechanical complexity. The OVR Series 3-axis SCARA's flat,  low-profile design allows it to operate inside these restricted spaces while still maintaining full horizontal reach and precise motion control.

From an engineering standpoint, a flatter design of the SCARA enables:

    • Closer robot placement to conveyors and cartons
    • Reduced need for custom mechanical extensions
    • Cleaner integration into existing packaging cells

Once the bottles are capped, they're placed on a "pallet" in the front.  Bottle placement locations are easily managed using a palletizing sequencing routine, ensuring consistent positioning and orientation with a variety of pallet patterns. For packaging engineers, this repeatability is critical; accurate downstream capping depends on every bottle arriving in the same location, cycle after cycle. Pallet-based motion programming is also easy and quick; ideal for future format changes while reducing commissioning and changeover time.

 

Step 2 Identify Variability with Machine Vision

Once the bottle is in position and ready to be capped, the system must address one of the most common challenges in packaging automation: arranging randomly oriented components.

Bottle caps rarely arrive in perfectly aligned positions. Rather than relying on bowl feeders or complex mechanical alignment, this system integrates a vision‑guided picking process using a Cognex 2800 series camera. The camera captures bottle cap locations and orientation data, which is then transmitted directly to our MRCU "all-in-one" integrated robot controller.  Without first acquiring this data from the vision camera, a robot cannot determine the location of the bottle cap.

This vision‑based approach offers several practical advantages:

    • Eliminates mechanical orientation tooling, reducing maintenance
    • Supports multiple cap styles and sizes
    • Improves flexibility for future product variants

For engineers designing automation cells, vision adds adaptability without sacrificing speed—assuming communication latency and coordinate transformations are handled correctly. In this system, tight integration between the camera, the robot controller, and the robot ensures accurate spatial mapping and consistent picking points.

 

Step 3 Bottle Cap Pick-and-Place with Vision-Integrated Articulated Robot

The OVR Series 4-Axis Articulated Robot on the left side performs the bottle cap pick-and-place operation from its supply bin to the bottle. Using real‑time vision data, it identifies the correct cap, picks it from its detected position, and accurately places it onto the waiting bottle.

Articulated robots excel in this type of operation because of their:

    • High repeatability in the XY plane
    • Fast cycle times
    • Stable vertical (Z‑axis) motion for controlled placement

Vision‑guided bottle capping requires more than just accurate picking.  It demands precise synchronization between motion axes, tooling, and placement force. Consistent vertical descent speeds, compliant tooling, or a torque control function can help prevent cross‑threading or damaged caps.

Can one robot perform both tasks?  From a system design perspective, separating bottle handling and cap placement across two robots allows:

    • Parallel task execution, improving throughput
    • Independent optimization of bottle handling and capping motions
    • Simpler troubleshooting and scalability

 

 Summary & Design Tips 

Together, the OVR Series 3-axis SCARA robot and the OVR Series 4-axis articulated robot create a compact, coordinated automation solution that combines mechanical accuracy with intelligent software control. Their unified operation integrates a low-profile robot design, machine vision, and coordinated motion to deliver a cell that can quickly adapt to changing product requirements without extensive re-engineering.

As packaging requirements continue to evolve, driven by shorter production runs, increased customization, and tighter space limitations, automation systems must be compact, intelligent, and highly flexible. Coordinated SCARA robots paired with vision systems provide a strong foundation for meeting today’s demands while maintaining the flexibility to support future changes.

 

OVR Series Small Industrial Robots Lineup

SCARA Robots

Articulated Robots

Cartesian / Gantry Robots

3-Axis

4-Axis

5-Axis

6-Axis

3-Axis

Built-in Reliability: All rotational joints and bases for the OVR Series robots are equipped with motors and rotary actuators from the AlphaSTEP Hybrid Step-Servo Product Family for closed-loop, absolute-position control.

 

Practical Design Tips from Our Application Engineer

    • Design for vertical constraints early: Low‑profile robots can unlock layouts that would otherwise require costly mechanical workarounds.
    • Use vision to manage variability, not just inspection: Vision‑guided robotics can replace mechanical orientation and increase flexibility.
    • Separate tasks to increase uptime: Dedicated robots for handling and placement simplify optimization and maintenance.
    • Plan for changeovers: Easy palletizing sequence programming and vision integration make future changes much easier to implement.

 

 

Topics: Robotics, VIDEOS, Application Examples, Food & Packaging, Bottle Capping, Product Demos, Factory Automation

Johann Tang

Written by Johann Tang

Johann Tang is a Product Specialist at Oriental Motor USA Corp. Before joining the marketing team, he spent 14 years in sales and technical application support, and he also led product training on various types of fractional-horsepower electric motors, gear motors, actuators, drivers, and controllers. If you have any questions, please feel free to use the live chat window, 1-800-GO-VEXTA (1-800-468-3982), or techsupport@orientalmotor.com, to reach our product support team. Sorry, comments have been turned off.

    Subscribe Here!

    Recent Posts

    New call-to-action