Engineering Notes by Oriental Motor

Explainer: How to Perform Wireless Motion Control with an Ethernet Type Driver

[fa icon="calendar"] Originally posted on Feb 28, 2025, 11:18:01 PM
Last updated on May 13, 2025 / by Johann Tang

Johann Tang

Explainer: How to Perform Wireless Motion Control with an Ethernet Type Driver
7:08

In the factories of the future, wireless motion control will offer unprecedented flexibility for mobile machines and space-constrained applications. This comprehensive guide walks engineers through implementing wireless motion control using Oriental Motor's AZ Series Ethernet Type mini Driver, eliminating cables while maintaining precise motion control.

What's covered?

  • Mertis of Wireless Motion Control
  • Required Components
  • Step-By-Step Instructions
  • Demo Video

Benefits of Wireless Motion Control

  • Design more mobile and flexible automation systems
  • Reduce cabling costs and complexity
  • Implement modular production lines
  • Integrate motion control with single-board computers or programming language, such as Rasberry Pi, Jetson, or Python

Mertis of Wireless Motion Control

The IIOT (Industrial Internet of Things) enables improved safety, increased efficiency, better decision-making, and faster response by collecting and analyzing data and automating tasks.   By eliminating cables, machines can be more mobile, compact, and less costly to make.  This can help AGVs and AMRs gain access to tight spaces, or customize production lines for different needs, such as in a modular automation concept.

 

Since Ethernet communication can be transmitted over Wi-Fi, wireless motion control, such as remote location control and status monitoring, can be performed with our AZ Series Ethernet Type mini Driver by using Modbus TCP communication protocol transmitted over an Ethernet cable to a Wi-Fi bridge.  This driver is part of our AlphaSTEP AZ Series product family, which means that it's compatible with a variety of DC-input motors, linear actuators, or rotary actuators.
 
In addition to our products, we'll also need a network router to create its own LAN network, a Wi-Fi bridge configured to bridge the router network to the driver via an Ethernet cable, and a laptop that can join the network and can exchange data with the driver over the network with our MEXE02 software (downloadable).  Once we add a motor, DC power supply, and cables, we can perform wireless motion control by remotely commanding the motor from the laptop.

 

Here's what you'll need:

  • 24 VDC power supply
    Brand: N/A
    P/N: N/A
Oriental Motor U.S.A. Corp.
  • AZ Series Ethernet type mini Driver
    P/N: AZD-KREN
  • AZ Series AlphaSTEP 60 mm motor
    P/N: AZM66AKH
  • Motor cable
    P/N: CCM002Z1EBF
  • "All-in-one" motor-driver bracket
    P/N: MAFP06W-6
  • Network Router
    Brand: Linksys
    P/N: EA6350
  • Wi-Fi Bridge
    Brand: Vonets
    P/N: VAP11G-300
Oriental Motor U.S.A. Corp.
  • MEXE02 Software (version 4.18.1 or later)
Amazon.com: The Dew Destroyer Destroyer Dew and Frost on Camera Lens all  night 60mm Strap + Large Capacity Battery : Electronics mounting brackets for az mini driver Product Image 1 of 4 MEXE02 Software

 

Required Components

Follow our detailed instructions to build your own wireless motion control system using readily available components and free software. 

 

 

Step-by-Step Instructions

1.  Set up the router

Connect the network router to the AC power supply.  After 30 seconds, the router's LED should flash green slowly (~every second).

 

2. Check the connections

Check the connections from the batteries to the driver's CN1 connector.  In our case, we used a terminal strip.
Check the connections from the batteries to the Wi-Fi bridge. 

Check the connections between the following:

  • Wi-Fi bridge and the driver
  • Motor and driver

 

3.  Power on and check LEDs (make sure the batteries are charged)

When powered, the Wi-Fi bridge's LED should be solid green initially, then start flashing blue quickly after ~15 seconds.  This means it has connected to the router network.

To charge batteries:

  • Turn batteries OFF
  • Unplug all connections (2 circular connections and 1 USB connection)
  • Plug in chargers to AC power and to batteries
  • Turn switches to the ON position
  • When charging is complete, the LEDs turn from red to green.

 

4.  Connect laptop to network

In the laptop's network settings, select the correct Wi-Fi bridge network.

 

5.  Open AZ Ethernet file in the MEXE02 software

In the MEXE02 software (version 4.18.1 or later), open an "AZ mini Ethernet type - Standard/Geared Motor" file.  Make sure to select the "AZ mini" Series.

 

6.  Configure your Ethernet connection setting on the MEXE02 software

Ethernet Connection Setting - Parameters

  • Select either Modbus TCP, Modbus UDP, or CC0Link IE field network protocols.
  • Enable "Support software connection (MEXE02)" by selecting "0".  This is necessary for first-time setup.
  • Save the "Port number (MEXE02)".  This will be needed later in the Ethernet connection setting.

 

Open your "Ethernet communication setting".

 

 

Ethernet Connection Setting - Parameters

 

 

  • Choose "Wi-Fi" for "Network adapter (PC)".
  • Set the driver's IP address either with dials or parameters (dial takes priority).
  • Make sure the "Destination port number" matches MEXE02's port number.
  • The host IP address should be in the same network as the driver, and the 1st three octets should be the same (ie: 192.1689.1.###).
  • Click "Apply" when done.
  • Ping driver to test if network communication is working properly.  You should receive 4 replies.

 

7.  Perform a data read operation to load the data. 

Close the communication settings.  You should be able to perform a "data read" operation, which uploads the stored data from the driver (if any).  If it reads correctly, you know you've set up the communication successfully.  If there's no stored data on the driver, you'll have to create a motion sequence data file.  Just fill in the values you want; like position (in steps), speed, starting/changing rate (acceleration rate), stopping deceleration (deceleration), operating current, type of link...etc.  If you don't fill some of the values in, it will use the default values instead.

 

 

8.  Perform a move, monitor motor status

Once you're done filling the values, remember to perform a "data write" operation to save the data into the driver.  Once the data is stored in the driver,  you can use the "Teaching, remote operation" to test any of the moves, jog the motor, and monitor the motor status at the same time.

 

 

Demo Video

Follow along as Paul Bosnyak, our senior application engineer, demonstrates how to perform wireless motion control with our AZ Series Ethernet type mini driver.

 

Additional Notes from Paul Bosnyak:

  • Ethernet driver allows for Ethernet connection. Many single-board PCs use Ethernet communication, so this can be integrated with a cost-effective host system, such as Raspberry Pi.
  • The router and Wi-Fi bridge need to be preconfigured during initial setup.
  • The Wi-Fi bridge does not create its own network but simply bridges the existing network created by the Linksys router. 
  • It is up to the customer (and their IT team) to determine necessary network security.

    Discover how combining Oriental Motor's precision motion technology with standard wireless networking creates powerful new possibilities for your next automation project.  Contact our team to set up a product consulation.

    Highlighted Product: AZ Series Ethernet Type mini Driver  

     

Topics: Stepper Motors, Robotics, Alphastep Hybrid Control, VIDEOS, Software, Network, Product Demos

Johann Tang

Written by Johann Tang

Johann Tang is a Product Specialist at Oriental Motor USA Corp. Before joining the marketing team, he spent 14 years in sales and technical application support, and he also led product training on various types of fractional-horsepower electric motors, gear motors, actuators, drivers, and controllers. If you have any questions, please feel free to use the live chat window, 1-800-GO-VEXTA (1-800-468-3982), or techsupport@orientalmotor.com, to reach our product support team. Sorry, comments have been turned off.

    Subscribe Here!

    Recent Posts

    New call-to-action