Engineering Notes by Oriental Motor

Improve Stepper Motor Performance Further with 3 Advanced Driver Features

[fa icon="calendar"] Originally posted on Dec 1, 2018, 12:00:00 PM
Last updated on May 19, 2026 / by Johann Tang

Johann Tang

There are many stepper motor manufacturers in the market place, but there are even more stepper motor driver manufacturers.  The crowded market place provides many standard product options for customers to build their motion control system just the way they like it. 

However, if the best possible performance is desired, it would be difficult to beat a tested combination of a specific motor and driver from the same manufacturer.  By combining R&D knowledge from both motors and drivers, unique product features can be developed to improve performance further.  

In this post, we discuss 3 advanced features of the CVD stepper motor drivers that were designed to improve the performance of the PKP Series high torque stepper motors: stable torque output even when microstepping, high efficiency components for high current output, and why buying both motors and drivers from the same manufacturer is better.

Consistent Torque Output Even When Microstepping 

Microstepping is a driver function that electrically subdivides the full step angle of a stepper motor in order to increase resolution or decrease vibration and noise.  Traditionally, inconsistent torque output or position accuracy are problems resulting from microstepping.  Due to individual motor phase current detectors as well as sine wave current drive technology, the CVD drivers can regulate torque more precisely even when microstepping.

Consistent torque output due to better current control

Learn how microstepping works


High Efficiency, Low Heat Design 

To increase the motor torque, the current from the driver to the motor must be increased.  However, increasing the current also increases the operating temperature for the driver, which can limit duty cycle or decrease life of the driver.  The CVD drivers utilized a low heat, high efficiency design, which makes it possible to apply a higher current to the motors.

  • Adoption of more efficient FETs for better heat transfer from the components to the PCB.  On resistance of new FETs are 1/20th of conventional FETs.
  • Improved heat transfer circuit board design helps minimize footprint.  No heat sink is required.

CVD driver FET and PCB

Conventional driver   CVD advanced microstepping driver
Conventional driver temperature distribution Reduce heat generation, increased torque CVD driver temperature distribution

With a stepper motor and driver that's rated for higher current, high speed torque can be increased without changing the motor size.  Here we show 2 PKP Series stepper motors of the same frame size and stack length.  By changing from a 2.8 A/phase winding to a 4.2 A/phase winding, we can increase the motor's torque output as seen in the speed torque curve.

NEMA 23 2-phase stepper motor 2.8 A/ph  Arrow NEMA 23 2-phase stepper motor 4.2 A/ph Increased torque with higher current

Unmatched Performance and Precision 

The CVD driver offers superior low vibration and noise characteristics by using a new, fully digital, full-time microstepping control circuit.  Current waveform and torque consistency are improved.  The Smooth Drive function provides quiet and smooth stepper motor performance that internally microsteps the basic step angle to a maximum resolution of 2048. 

cvd-driver-reduced-vibration-1

The CVD drivers are equipped with multiple functions to suppress different types of vibrations that happen at different speed ranges; such as typical ringing from step movements that happen at low speeds, resonance and torque ripples at medium speeds, and vibrations that are caused by back EMF at high speeds. 

Since some functions use specific motor winding data that are proprietary, this kind of performance is only possible by pairing a motor and a driver from the same manufacturer. 

CVD driver vibration comparison

As a result, the CVD drivers can provide unmatched stepper motor performance with significantly reduced vibration and noise.

In general, the stop accuracy of stepper motors is worse when microstepping since microstepping requires highly precise current control from the driver.  With better current control from the CVD driver, the stepper motor can actually perform better than its standard specification of ±3 arc minutes (±0.05º).

Stepper motor vibration comparison

Watch the following video to learn how the CVD drivers can improve the performance of stepper motors.

If you wish to learn more about the features of our CVD driver in depth, please read our white paper.

Watch related product videos or size your next stepper motor with our motor sizing tool.

 

There are multiple product lines of CVD drivers. 
If you need help, please discuss your requirements with our team.

CVD Drivers for 2-Phase Stepper Motors

CVD Drivers for 5-Phase Stepper Motors

CVK-SC Series Speed Control Stepper Motors

Building your own?  Ask about the S-Type Board Mounting Type driver

New call-to-action

 

Topics: Stepper Motors, Smooth Drive, VIDEOS, Product Introductions, Stepper Drivers, Incremental Positioning

Johann Tang

Written by Johann Tang

Johann Tang is a Product Specialist at Oriental Motor USA Corp. Before joining the marketing team, he spent 14 years in sales and technical application support, and he also led product training on various types of fractional-horsepower electric motors, gear motors, actuators, drivers, and controllers. If you have any questions, please feel free to use the live chat window, 1-800-GO-VEXTA (1-800-468-3982), or techsupport@orientalmotor.com, to reach our product support team. Sorry, comments have been turned off.

    Subscribe Here!

    Recent Posts

    New call-to-action