Engineering Notes by Oriental Motor

Wattage Specification for Stepper Motors

[fa icon="calendar"] Originally posted on May 31, 2023, 7:56:20 PM
Last updated on May 19, 2026 / by Johann Tang

Johann Tang

Historically, stepper motors are not rated by watts like AC motors or servo motors.  So...how would you compare a stepper motor to a servo motor or a brushless motor?

 

Teruyo (stepper wattage)

 

The reason why stepper motors are not rated in watts is because there is no concept of rated rotation speed (RPM) for stepper motors.

 

Why do we need the rated speed?

AC motors and servo motors are rated for maximum power, in watts, at their rated speeds.  Since stepper motors don't have a standard rated speed value, Oriental Motor does not show a wattage specification for stepper motors.  If necessary, the wattage value can be calculated.

 

Formula for output watts

Output [W] = 2 × π × T × N ≒ 0.1047 × T × N

60

= 0.1047 x T x N

0.1047: Constant
T [N m]: Torque
N [r/min]: Rotation speed

 

How do you choose the rated speed?

Even though there is no rated speed for stepper motors, it's theoretically possible to derive the output wattage from the formula above based on the operating speed.  However, the output watts value will change according to the rated speed you choose.

Here's a general reference for other types of motors:

  • AC small standard motor: 1,500 r/min at 60Hz (depends on model)
  • Brushless motor: 3,000 r/min (depends on model)
  • AC servo motor: 3,000 r/min

 

Let's look at some examples.

 

●PKE566AC motor + RKSD507-AD driver (RKS566AA system) speed - torque characteristics

 

RKS566 speed torque curve

 

1.  0.1047 x 0.5 x 1000 = 52.3 W when calculated with a rotation speed of 1000 r/min and a torque of 0.5 Nm.*
2.  0.1047 x 0.2 x 3000 = 62.8 W when calculated with a rotation speed of 3000 r/min and a torque of 0.2 Nm.*
*The red arrows only go up half way to the speed-torque curve because the safety factor is typically 2:1 by default for stepper motors, so the selection was made so that the pullout torque is not exceeded when the required torque is doubled.

 

Let's look at another example.  How about comparing servo motors to brushless motors?

 

●BXM230-A2 motor + BXSD30-A2 driver (BXS230A-A system) speed - torque characteristics

BXM230-A2 speed torque curve
1.  When calculated at a rotation speed of 1000 r/min: 0.1047 x 0.1 x 1000 ≒ 10W. 
2.  When calculated at a rotation speed of 3000 r/min: 0.1047 x 0.1 x 3000 ≒ 30W.
TIP When comparing stepper motors to either servo motors or brushless motors, keep in mind that servo motors or brushless motors offer an instantaneous max torque for a limited time.  Stepper motors typically do not offer this.

 

Don't feel like calculating? 

Here's a quick reference chart comparing our AlphaStep AZ Series closed-loop stepper motors with servo motors with equivalent output.

Example: AZ series stepper motors

AZ series (standard type)
Servo motor with equivalent rated torque (reference)
Frame size Part number
42mm AZM46 Equivalent to rated torque of 50 to 100W
AZM48
60mm AZM66 Equivalent to rated torque of 100 to 200W
AZM69 Equivalent to rated torque of 200 to 400W
85mm AZM98 Equivalent to rated torque of 400 to 750W
AZM911

 

If you're wondering, here's a comparison of speed-torque curves between a closed-loop stepper motor and a servo motor of equivalent output.

 

AlphaStep Rated Output

 

For comparisons of other sizes, please refer to https://www.orientalmotor.co.jp/products/stepping/overview_5/.  Sorry, only Japanese is available at this time.  I will try to update this post as they become available.  In the mean time, please use Google Translate to translate the page.

 

Also, be aware of the fundamental and performance differences between stepper motors and servo motors.  For example, servo motors work best for rigid mechanical setups at high speeds (ie: ball screw), and stepper motors work best for more compliant setups at low to medium speeds (ie: belt and pulley).  To learn more, please read this blog post, The Choice Between Servo Motors and Stepper Motors.

 

Pick the right motor the first time!  Contact our technical support engineers for a product sizing consultation.

Contact Our Experts

 

Topics: Stepper Motors

Johann Tang

Written by Johann Tang

Johann Tang is a Product Specialist at Oriental Motor USA Corp. Before joining the marketing team, he spent 14 years in sales and technical application support, and he also led product training on various types of fractional-horsepower electric motors, gear motors, actuators, drivers, and controllers. If you have any questions, please feel free to use the live chat window, 1-800-GO-VEXTA (1-800-468-3982), or techsupport@orientalmotor.com, to reach our product support team. Sorry, comments have been turned off.

    Subscribe Here!

    Recent Posts

    New call-to-action