Engineering Notes by Oriental Motor

Welcome to Oriental Motor's "Engineering Notes" Blog:

Products and technology are only valuable when coupled with skilled people and services to support them. Since 1978, ORIENTAL MOTOR U.S.A. CORP. has been building a service and support system to better serve customers. It is our goal to provide the best product and service from the design phase, through the sale and beyond.

Our blog will feature:

  • Introduction to new products and technologies
  • Motion control basics and application examples
  • Tips for motor selection, programming, and troubleshooting

 

Incremental Encoders vs Absolute Encoders

Posted by Johann Tang on Sep 12, 2019, 3:57:57 PM

The terms "absolute" and "incremental" come up frequently in the world of position control.  The exact meaning can be the type of motion done by the motor in programming terms or the type of feedback device used with the motor.  In this article, we will focus on the differences between an incremental closed-loop feedback system and an absolute closed-loop feedback system.

Read More

Topics: Stepper Motors, Absolute Positioning, Alphastep Hybrid Control, Linear Actuators, VIDEOS

A Brief Overview of the AlphaStep Family

Posted by Johann Tang on Aug 28, 2019, 2:37:43 PM

AlphaStep Logo

The word, "AlphaStep", describes Oriental Motor's patented Hybrid Control technology, which offers improved stepper motor performance by sensing the rotor position and automatically switching between open-loop and closed-loop operation when necessary.  This post explains the unique technologies offered within the AlphaStep family of products and summarizes the numerous integrated options available.  It also can serve as a website navigation guide (video added).

Read More

Topics: Stepper Motors, Absolute Positioning, Alphastep Hybrid Control, Linear Actuators, VIDEOS, Gearheads, Software, Network

How Easy Is It to Build a Robot?

Posted by Johann Tang on Jul 19, 2019, 8:31:19 PM

Robot adoption is increasing in many industries due to global efforts in reducing long term costs, maintaining quality, and freeing up time for humans to do "human" tasks.  For example, by using a robot to clean floors or restock shelves in a supermarket, human employees can spend more time helping or selling to their customers.  A company can either tap into this robotic trend by buying ready-made robots, or by making their own with less cost. 

If engineering resources are limited, selecting the right components can reduce the difficulty and time for building a robot.

Read More

Topics: Stepper Motors, Robotics, Absolute Positioning, Alphastep Hybrid Control, Linear Actuators, Motor Sizing, VIDEOS, Gearheads, Software, Application Examples

Benefits of an Absolute Rack and Pinion System Compared to Other Linear Motion Mechanisms

Posted by Johann Tang on Jul 2, 2019, 3:25:24 PM

There are many mechanisms that convert rotary motion of an electric motor to linear motion, such as belt/chain drives, screw drives, rack & pinion drives and even CAM drives.  Each mechanism offers advantages and disadvantages. Choosing the right technology can help increase load, speed, travel distance, or positioning accuracy.

Read More

Topics: Absolute Positioning, Alphastep Hybrid Control, Linear Actuators, VIDEOS, Vertical Lifts, Application Examples

Simple Method to Limit Motor Operation Range for Robotics Safety

Posted by Johann Tang on Apr 1, 2019, 2:09:05 PM

In the world of industrial robotics, there are several types of robots typically offering multiple axes of motion for tasks such as parts assembly, material handling, or pick and place operations.  These include articulated robots, cartesian/gantry robots, SCARA robots, and Delta robots.  Variations of end effectors such as grippers, welders or part rotators can be mounted on the end of the arm to perform different tasks.  Depending on number of axes or load capacity, costs can easily add up.  Limiting the operation range for these robotic axes of motion is an easy way to prevent costly problems or safety issues later.

Read More

Topics: Stepper Motors, Robotics, Absolute Positioning, Alphastep Hybrid Control, VIDEOS, Software, Application Examples

Wrap Function: Simplified Position Control for Rotary Indexing in Absolute Coordinates

Posted by Johann Tang on Jan 4, 2019, 7:56:17 PM

With recent trends focusing on improving engineering efficiency, many products have been developed to specifically help shorten design cycles for machine automation.  Part of improving efficiency is making products easier to use, so additional time and resources can be spent elsewhere.  This post describes a product feature that can make index table applications less complex to manage.

Read More

Topics: Stepper Motors, Absolute Positioning, Linear Actuators, VIDEOS, Software, Application Examples

Smart System Performs Reciprocating Motion & Force Sensing Without a PLC or External Sensors

Posted by Johann Tang on Oct 30, 2018, 1:38:20 PM

Automation is great for repetitive tasks, such as test fixtures for a process that has to repeated.  In this post, we will explain how to perform a reciprocating motion (back and forth cycles) with a product that does not require a PLC or external presence sensors, which can help speed up design cycles.

Read More

Topics: Torque Limit (Push Motion, Tension Control), Absolute Positioning, Alphastep Hybrid Control, Linear Actuators, VIDEOS, Software, Application Examples

    Subscribe Here!