Engineering Notes by Oriental Motor

Welcome to Oriental Motor's "Engineering Notes" Blog:

Products and technology are only valuable when coupled with skilled people and services to support them. Since 1978, ORIENTAL MOTOR U.S.A. CORP. has been building a service and support system to better serve customers. It is our goal to provide the best product and service from the design phase, through the sale and beyond.

Our blog will feature:

  • Introduction to new products and technologies
  • Motion control basics and application examples
  • Tips for motor selection, programming, and troubleshooting

 

The Right Motor for Tension Control

Posted by Johann Tang on Sep 1, 2022 12:00:00 PM

Tension control is a niche application that is not easy to implement.  Using the right type of motor is the first step to success.  Hint: you don't always have to use a servo motor.

Read More

Topics: AC Motors, Torque Limit (Push Motion, Tension Control)

Torque Limit Application Example - Bottle Capping with BLDC Motors

Posted by Johann Tang on Feb 15, 2019 1:00:00 PM

For applications where torque needs to be limited, an external mechanical torque limiter is typically required in addition to the motor system.  When the torque exceeds the limit, the torque limiter will either decouple the load or limit the torque by slipping.  An electric motor system's built-in torque limit function can simplify machine designs by eliminating this extra component.

Read More

Topics: Torque Limit (Push Motion, Tension Control), Speed Control, VIDEOS, BLDC Motors, Application Examples, Food & Packaging, Bottle Capping

Improve Gripping Operation with Multiple Torque Limit Settings

Posted by Johann Tang on Jan 15, 2019 1:00:00 PM

Robotic grippers are typically used to grip parts for transport.  The driving force behind a gripper can be pneumatic, hydraulic, or electric.  Which type is best for gripping?

Read More

Topics: Torque Limit (Push Motion, Tension Control), Robotics, Speed Control, VIDEOS, BLDC Motors, Application Examples, Medical, Grip Conveyors

Smart System Performs Reciprocating Motion & Force Sensing Without a PLC or External Sensors

Posted by Johann Tang on Oct 30, 2018 1:38:20 PM

Automation is great for repetitive tasks, such as test fixtures for a process that has to repeated.  In this post, we will explain how to perform a reciprocating motion (back and forth cycles) with a product that does not require a PLC or external presence sensors, which can help speed up design cycles.

Read More

Topics: Torque Limit (Push Motion, Tension Control), Absolute Positioning, Alphastep Hybrid Control, Linear Actuators, VIDEOS, Software, Application Examples

    Subscribe Here!