Engineering Notes by Oriental Motor

Welcome to Oriental Motor's "Engineering Notes" Blog:

Products and technology are only valuable when coupled with skilled people and services to support them. Since 1978, ORIENTAL MOTOR U.S.A. CORP. has been building a service and support system to better serve customers. It is our goal to provide the best product and service from the design phase, through the sale and beyond.

Our blog will feature:

  • Introduction to new products and technologies
  • Motion control basics and application examples
  • Tips for motor selection, programming, and troubleshooting

 

Monitor Your Machine Like a Traffic Light System

Posted by Johann Tang on Jun 19, 2020, 8:00:00 PM

For automated factories, motor failures mean lost production and lost revenue.  Being able to identify the specific issue in advance and its location is critical to maintaining production efficiency.  To be successful, extra sensors must be added to detect abnormalities.  There may be an easier way.

Read More

Topics: Stepper Motors, Alphastep Hybrid Control, Linear Actuators, VIDEOS, Network, Application Examples, Troubleshooting, Factory Automation

Flexible Configurations For Hollow Rotary Actuators

Posted by Johann Tang on May 21, 2020, 11:30:00 AM

Read More

Topics: Stepper Motors, Robotics, Absolute Positioning, Alphastep Hybrid Control, Linear Actuators, Gearheads, Rotary Actuators/Index Tables

Control Basics: The Difference Between Sink and Source Logic

Posted by Johann Tang on Apr 30, 2020, 9:16:14 PM

For someone who has never had experience wiring I/O for motion control, it can be scary the first time.  If devices are not wired correctly, it can cause a range of issues from a motor simply not doing what's expected to irreversible product damage.  I still get that nervous feeling before I press the START button on a demo.  Murphy's Law, anyone?

Read More

Topics: AC Motors, Stepper Motors, Alphastep Hybrid Control, Linear Actuators, Speed Control, BLDC Motors, Servo Motors, Motion Control Basics

The Proper Way to Use a Gripper

Posted by Johann Tang on Mar 5, 2020, 5:11:16 PM

A gripper is typically an end effector that is installed at the end of a robotic arm or on a cartesian robot and can be used to grip parts in order to transfer them from one location to another.  However, there's more to it than just closing the jaws to pinch a part.  

Read More

Topics: Stepper Motors, Robotics, Absolute Positioning, Alphastep Hybrid Control, Linear Actuators, VIDEOS, Application Examples

Motor Sizing Basics Part 3: How to Calculate Speed, Acceleration Torque, and RMS Torque

Posted by Johann Tang on Feb 27, 2020, 9:05:40 PM

Now that we understand the calculations behind load torque and load inertia, we're a little closer to motor selection.  You might be wondering why I separated load torque and acceleration torque calculations.  That's because in order to calculate for acceleration torque, load inertia and speed must be calculated first. 

Read More

Topics: AC Motors, Stepper Motors, Alphastep Hybrid Control, Linear Actuators, Speed Control, Motor Sizing, BLDC Motors, Servo Motors, Motion Control Basics

Motor Sizing Basics Part 2: How to Calculate Load Inertia

Posted by Johann Tang on Jan 17, 2020, 7:51:53 PM

Other than torque or speed, another factor should be considered when sizing motors.  

Read More

Topics: AC Motors, Stepper Motors, Alphastep Hybrid Control, Linear Actuators, Speed Control, Motor Sizing, BLDC Motors, Gearheads, Servo Motors, Rotary Actuators/Index Tables, Motion Control Basics

Motor Sizing Basics Part 1: How to Calculate Load Torque

Posted by Johann Tang on Jan 14, 2020, 8:14:54 PM

Proper sizing of a motor requires that 3 criteria must be met: torque, load inertia, and speed.  For the first part of this Motor Sizing Basics series, I will be explaining what load torque is, how to calculate it for specific application examples, and how it fits into the torque requirement for the application.

Read More

Topics: AC Motors, Stepper Motors, Alphastep Hybrid Control, Linear Actuators, Speed Control, Motor Sizing, BLDC Motors, Servo Motors, Rotary Actuators/Index Tables, Motion Control Basics, Conveyors

Incremental Encoders vs Absolute Encoders

Posted by Johann Tang on Sep 12, 2019, 3:57:57 PM

The terms "absolute" and "incremental" come up frequently in the world of position control.  The exact meaning can be the type of motion done by the motor in programming terms or the type of feedback device used with the motor.  In this article, we will focus on the differences between an incremental closed-loop feedback system and an absolute closed-loop feedback system.

Read More

Topics: Stepper Motors, Absolute Positioning, Alphastep Hybrid Control, Linear Actuators, VIDEOS

A Brief Overview of the AlphaStep Family

Posted by Johann Tang on Aug 28, 2019, 2:37:43 PM

AlphaStep Logo

The word, "AlphaStep", describes Oriental Motor's patented Hybrid Control technology, which offers improved stepper motor performance by sensing the rotor position and automatically switching between open-loop and closed-loop operation when necessary.  This post explains the unique technologies offered within the AlphaStep family of products and summarizes the numerous integrated options available.  It also can serve as a website navigation guide (video added).

Read More

Topics: Stepper Motors, Absolute Positioning, Alphastep Hybrid Control, Linear Actuators, VIDEOS, Gearheads, Software, Network

Reactive vs Preventive vs Predictive Maintenance: Why Predictive Maintenance is Better

Posted by Johann Tang on Aug 20, 2019, 2:58:24 PM

Along with the advancement of industrial technology, maintenance methods of motion control components of a machine, such as motors, drives, and sensors, have also evolved.

Most of us still use the traditional "reactive" maintenancemethod in many aspects of life, such as replacing a dishwasher in your kitchen.  People don't buy a dishwasher until theirs doesn't work anymore.  Well, for factories that rely on consistent uptime for production, this wasn't the best strategy.  Realizing the need for improvement, maintenance personnel started to estimate life and replace motion control components before they failed.  This is called the "preventive" maintenancemethod, which also wasn't a perfect strategy for cost.  More recently, with the advancement of IIoT (Industrial Internet of Things) technologies and real-time availability of status data, another method was made possible - the "predictive" maintenance method.

Read More

Topics: Stepper Motors, Linear Actuators, VIDEOS, Network, Application Examples

    Subscribe Here!