Engineering Notes by Oriental Motor

Welcome to Oriental Motor's "Engineering Notes" Blog:

Products and technology are only valuable when coupled with skilled people and services to support them. Since 1978, ORIENTAL MOTOR U.S.A. CORP. has been building a service and support system to better serve customers. It is our goal to provide the best product and service from the design phase, through the sale and beyond.

Our blog will feature:

  • Introduction to new products and technologies
  • Motion control basics and application examples
  • Tips for motor selection, programming, and troubleshooting

 

How the OVR Series SCARA Robots Improve Design, Accessibility, and Throughput for Laboratory Automation

Posted by Johann Tang on Aug 28, 2026, 5:45:00 PM

How the OVR Series SCARA Robots Improve Design, Accessibility, and Throughput for Laboratory Automation
12:14

As laboratory automation and diagnostic equipment become more compact and increasingly dense, robot selection is no longer driven solely by reach and payload.  Space constraints often dictate machine architecture just as much as performance requirements.  Engineers need robots that can operate efficiently in tight spaces without sacrificing speed, payload, or flexibility.

Read More

Topics: Robotics, Absolute Positioning, VIDEOS, Application Examples, Medical

Why Electromagnetic Brake Type Motors are Necessary for the Medical Industry

Posted by Johann Tang on Mar 31, 2025, 9:00:00 PM

Why Electromagnetic Brake Type Motors are Necessary for the Medical Industry
8:34

Motors with built-in electromagnetic brakes enhance safety by preventing unexpected movement during power failures, which is crucial for medical applications where precision, safety, and reliability are essential.
 
Read More

Topics: AC Motors, Stepper Motors, Robotics, Absolute Positioning, Linear Actuators, VIDEOS, BLDC Motors, Vertical Lifts, Application Examples, Service Life, Medical, Laboratory, Incremental Positioning

Stepper Motor Linear Actuator Attachment: Easily Convert Stepper Motors to Linear Actuators

Posted by Johann Tang on Sep 30, 2024, 12:00:00 PM

Stepper Motor Linear Actuator Attachment: Easily Convert Stepper Motors to Linear Actuators
6:15

 

The popularity of micro linear actuators has been steadily increasing, driven by the need to increase productivity in confined spaces.  To help meet the demand of the miniaturization trend, Oriental Motor has developed a compact linear actuator that can be attached to an off-the-shelf stepper motor.

Read More

Topics: Stepper Motors, Robotics, Absolute Positioning, Linear Actuators, VIDEOS, Application Examples, Product Introductions, Medical, Incremental Positioning

Case Study: How a Compact Electric Gripper Can Help with Articulated Robots

Posted by Johann Tang on May 31, 2024, 8:45:00 AM

Case Study: How a Compact Electric Gripper Can Help with Articulated Robots
14:17

An end effector, such as an electric gripper, is an essential part of industrial robots. More importantly, using the right gripper for the load being transferred prevents damage while improving automation efficiency.  In this article, we share how one system integrator has successfully adopted an electric gripper for one of their articulated robots.

Read More

Topics: Robotics, Absolute Positioning, Alphastep Hybrid Control, Linear Actuators, VIDEOS, Application Examples, Medical, Food & Packaging, Case Studies, Factory Automation

Improve Positioning Precision for Autosamplers with High Resolution and Encoder Type Stepper Motors

Posted by Johann Tang on Sep 26, 2023, 2:54:58 PM

In this article, we're diving deeper into two stepper motor types: high-resolution type and encoder type; and how they can be used to improve precision in critical laboratory automation applications like autosamplers.

Read More

Topics: Stepper Motors, VIDEOS, Application Examples, Encoders, XYZ/Cartesian/Gantry, Medical, Laboratory, Incremental Positioning

Peristaltic Pump Motor Selection Tips: Brushless Motor or Stepper Motor?

Posted by Johann Tang on Jun 26, 2023, 8:15:00 PM

This article highlights the advantages of brushless motors and stepper motors for driving a peristaltic pump, which is among the most common motor applications in medical, pharmaceutical, biotech, and diagnostic equipment.  

Read More

Topics: Stepper Motors, Speed Control, BLDC Motors, Pumps, Application Examples, Medical

Better Motor Alternatives for Variable Speed Pumps

Posted by Johann Tang on May 6, 2019, 8:03:26 PM

What motors do you use for pumps?  For variable speed pump applications that typically use 3-phase AC induction motors with variable frequency drives (VFDs), there is another type of motor that can transfer fluids more consistently and help reduce footprint.

Read More

Topics: AC Motors, Speed Control, VIDEOS, BLDC Motors, Pumps, Application Examples, Medical

Improve Gripping Operation with Multiple Torque Limit Settings

Posted by Johann Tang on Jan 15, 2019, 1:00:00 PM

Robotic grippers are typically used to grip parts for transport.  The driving force behind a gripper can be pneumatic, hydraulic, or electric.  Which type is best for gripping?

Read More

Topics: Torque Limit (Push Motion, Tension Control), Robotics, Speed Control, VIDEOS, BLDC Motors, Application Examples, Medical, Grip Conveyors

Easily Synchronize Speeds of Multiple Motors

Posted by Johann Tang on Oct 15, 2018, 9:00:00 AM

There are a variety of ways to synchronize the speed of multiple motors.  In this blog post, we will explain another advantage of using brushless motors systems, which is its ability to set speeds accurately and be able to synchronize speeds on multiple axes easily .  Brushless motors utilize built-in hall-effect sensors to regulate speed.  Even if the load, input voltage, or temperature fluctuates, the speed regulation will always be under +/-0.2% or better.

Read More

Topics: AC Motors, Speed Control, VIDEOS, BLDC Motors, Washdown, Application Examples, Medical, Food & Packaging, Grip Conveyors, Conveyors

Designing Smaller and Lighter Conveyors With Brushless Motors

Posted by Johann Tang on Oct 1, 2018, 8:32:18 AM

With the growing popularity of efficient brushless motors, replacing AC motors with these motors brings several advantages.  In this blog post, we will uncover one of the advantages that can benefit lighter and compact equipment designs. 

Read More

Topics: AC Motors, Speed Control, VIDEOS, BLDC Motors, Washdown, Application Examples, Medical, Food & Packaging, Grip Conveyors, Conveyors, Factory Automation

    Subscribe Here!