An AC motor can be simple to use, but its speed changes according to the size of the load or amount of voltage supplied. For an application where keeping a uniform speed is important, there is another type of motor that can improve performance.
Welcome to Oriental Motor's "Engineering Notes" Blog:
Products and technology are only valuable when coupled with skilled people and services to support them. Since 1978, ORIENTAL MOTOR U.S.A. CORP. has been building a service and support system to better serve customers. It is our goal to provide the best product and service from the design phase, through the sale and beyond.
Our blog will feature:
- Introduction to new products and technologies
- Motion control basics and application examples
- Tips for motor selection, programming, and troubleshooting
Eliminate Motor Speed Fluctuations Caused By Input Voltage or Load Variance
Topics: AC Motors, Speed Control, VIDEOS, BLDC Motors, Application Examples
Are you using motors for a start/stop conveyor or similar application? While AC motors are a common choice for conveyors, there is a unique speed control motor solution available that could improve stop accuracy as well as reduce footprint and cost of machine designs.
Topics: AC Motors, Stepper Motors, Speed Control, VIDEOS, Application Examples, Conveyors, Incremental Positioning, Factory Automation
What motors do you use for pumps? For variable speed pump applications that typically use 3-phase AC induction motors with variable frequency drives (VFDs), there is another type of motor that can transfer fluids more consistently and help reduce footprint.
Topics: AC Motors, Speed Control, VIDEOS, BLDC Motors, Pumps, Application Examples, Medical
Right Angle Gearheads: Why are Hypoid Gears Better Than Worm Gears?
As efficiency becomes increasingly important, another type of gear is being adopted for right-angle gearheads over the common worm gears.
Topics: AC Motors, Speed Control, BLDC Motors, Gearheads
Simple Method to Limit Motor Operation Range for Robotics Safety
In the world of industrial robotics, there are several types of robots typically offering multiple axes of motion for tasks such as parts assembly, material handling, or pick and place operations. These include articulated robots, cartesian/gantry robots, SCARA robots, and Delta robots. Variations of end effectors such as grippers, welders or part rotators can be mounted on the end of the arm to perform different tasks. Depending on number of axes or load capacity, costs can easily add up. Limiting the operation range for these robotic axes of motion is an easy way to prevent costly problems or safety issues later.
Topics: Stepper Motors, Robotics, Absolute Positioning, Alphastep Hybrid Control, VIDEOS, Software, Application Examples
Introduction to the MEXE02 Universal Motion Control Support Software
The MEXE02 support software is a universal motion control and monitor software used with multiple products from Oriental Motor, such as the AZ Series, RK2 Series, BLE2 Series, and BX2 Series. This article is useful for first-time users to gain a quick understanding of the software and what it can do.
Topics: Stepper Motors, Linear Actuators, Speed Control, VIDEOS, BLDC Motors, Software, Servo Motors
Torque Limit Application Example - Bottle Capping with BLDC Motors
For applications where torque needs to be limited, an external mechanical torque limiter is typically required in addition to the motor system. When the torque exceeds the limit, the torque limiter will either decouple the load or limit the torque by slipping. An electric motor system's built-in torque limit function can simplify machine designs by eliminating this extra component.
Topics: Torque Limit (Push Motion, Tension Control), Speed Control, VIDEOS, BLDC Motors, Application Examples, Food & Packaging, Bottle Capping
Flexible Mounting Options for Compact Stepper Motor Drivers
A driver is a must-have for any stepper motor. In a stepper motor system, a driver controls how the motor operates based on signals received from the controller. It is responsible for sending current through various phases in a stepper motor and also regulates the motor current (torque) and step resolution. With recent trends of minimizing machine footprint, finding space to install drivers could be challenging.
Standard Stepper Motor System Configuration
Topics: Stepper Motors, VIDEOS, Application Examples, Stepper Drivers, Incremental Positioning
Improve Gripping Operation with Multiple Torque Limit Settings
Robotic grippers are typically used to grip parts for transport. The driving force behind a gripper can be pneumatic, hydraulic, or electric. Which type is best for gripping?
Topics: Torque Limit (Push Motion, Tension Control), Robotics, Speed Control, VIDEOS, BLDC Motors, Application Examples, Medical, Grip Conveyors
Wrap Function: Simplified Position Control for Rotary Indexing in Absolute Coordinates
With recent trends focusing on improving engineering efficiency, many products have been developed to specifically help shorten design cycles for machine automation. Part of improving efficiency is making products easier to use, so additional time and resources can be spent elsewhere. This post describes a product feature that can make index table applications less complex to manage.
Topics: Stepper Motors, Absolute Positioning, Linear Actuators, VIDEOS, Software, Application Examples