Engineering Notes by Oriental Motor

Welcome to Oriental Motor's "Engineering Notes" Blog:

Products and technology are only valuable when coupled with skilled people and services to support them. Since 1978, ORIENTAL MOTOR U.S.A. CORP. has been building a service and support system to better serve customers. It is our goal to provide the best product and service from the design phase, through the sale and beyond.

Our blog will feature:

  • Introduction to new products and technologies
  • Motion control basics and application examples
  • Tips for motor selection, programming, and troubleshooting

 

Torque Limit Application Example - Bottle Capping with BLDC Motors

Posted by Johann Tang on Feb 15, 2019, 1:00:00 PM

For applications where torque needs to be limited, an external mechanical torque limiter is typically required in addition to the motor system.  When the torque exceeds the limit, the torque limiter will either decouple the load or limit the torque by slipping.  An electric motor system's built-in torque limit function can simplify machine designs by eliminating this extra component.

Read More

Topics: Torque Limit (Push Motion, Tension Control), Speed Control, VIDEOS, BLDC Motors, Application Examples, Food & Packaging, Bottle Capping

Flexible Mounting Options for Compact Stepper Motor Drivers

Posted by Johann Tang on Feb 1, 2019, 11:00:00 AM

A driver is a must-have for any stepper motor.  In a stepper motor system, a driver controls how the motor operates based on signals received from the controller.  It is responsible for sending current through various phases in a stepper motor and also regulates the motor current (torque) and step resolution.  With recent trends of minimizing machine footprint, finding space to install drivers could be challenging.

Standard Stepper Motor System Configuration

Read More

Topics: Stepper Motors, VIDEOS, Application Examples, Stepper Drivers, Incremental Positioning

Improve Gripping Operation with Multiple Torque Limit Settings

Posted by Johann Tang on Jan 15, 2019, 1:00:00 PM

Robotic grippers are typically used to grip parts for transport.  The driving force behind a gripper can be pneumatic, hydraulic, or electric.  Which type is best for gripping?

Read More

Topics: Torque Limit (Push Motion, Tension Control), Robotics, Speed Control, VIDEOS, BLDC Motors, Application Examples, Medical, Grip Conveyors

Wrap Function: Simplified Position Control for Rotary Indexing in Absolute Coordinates

Posted by Johann Tang on Jan 4, 2019, 7:56:17 PM

With recent trends focusing on improving engineering efficiency, many products have been developed to specifically help shorten design cycles for machine automation.  Part of improving efficiency is making products easier to use, so additional time and resources can be spent elsewhere.  This post describes a product feature that can make index table applications less complex to manage.

Read More

Topics: Stepper Motors, Absolute Positioning, Linear Actuators, VIDEOS, Software, Application Examples

Accelerate Design Cycles for Mobile Robots With Standard Features & Functions

Posted by Johann Tang on Dec 15, 2018, 12:00:00 PM

In the market of electric motors, there are products designed for general purpose applications, and there are motors designed for specialized applications, such as automated guided vehicles (AGVs) or autonomous mobile robots (AMRs).  While standard, general-purpose motors work for most applications such as factory automation, sometimes, it may help accelerate your design cycle by going with a motor system that already offers the features that you are planning to design into your machine.  In this post, we will summarize some of these features.

Read More

Topics: Robotics, Speed Control, Motor Sizing, BLDC Motors, Gearheads, Application Examples, AGV/AMR

Choosing the Right Type of Stepper Motor for Your Application

Posted by Johann Tang on Nov 12, 2018, 8:30:00 AM

Stepper motors are popular for their ability to stop accurately as well as their ease of use.  Both the amount of rotation and the speed are controlled easily with the same digital square wave pulse signal.  Unlike servo motors, stepper motors do not need an encoder to operate.  Example applications of stepper motors are CNC machines, index tables, robotics, scanners, and more recently, 3D printers.

Read More

Topics: Stepper Motors, Motor Sizing, VIDEOS, Application Examples, Motion Control Basics, Encoders, Incremental Positioning

Smart System Performs Reciprocating Motion & Force Sensing Without a PLC or External Sensors

Posted by Johann Tang on Oct 30, 2018, 1:38:20 PM

Automation is great for repetitive tasks, such as test fixtures for a process that has to repeated.  In this post, we will explain how to perform a reciprocating motion (back and forth cycles) with a product that does not require a PLC or external presence sensors, which can help speed up design cycles.

Read More

Topics: Torque Limit (Push Motion, Tension Control), Absolute Positioning, Alphastep Hybrid Control, Linear Actuators, VIDEOS, Software, Application Examples

Easily Synchronize Speeds of Multiple Motors

Posted by Johann Tang on Oct 15, 2018, 9:00:00 AM

There are a variety of ways to synchronize the speed of multiple motors.  In this blog post, we will explain another advantage of using brushless motors systems, which is its ability to set speeds accurately and be able to synchronize speeds on multiple axes easily .  Brushless motors utilize built-in hall-effect sensors to regulate speed.  Even if the load, input voltage, or temperature fluctuates, the speed regulation will always be under +/-0.2% or better.

Read More

Topics: AC Motors, Speed Control, VIDEOS, BLDC Motors, Washdown, Application Examples, Medical, Food & Packaging, Grip Conveyors, Conveyors

Designing Smaller and Lighter Conveyors With Brushless Motors

Posted by Johann Tang on Oct 1, 2018, 8:32:18 AM

With the growing popularity of efficient brushless motors, replacing AC motors with these motors brings several advantages.  In this blog post, we will uncover one of the advantages that can benefit lighter and compact equipment designs. 

Read More

Topics: AC Motors, Speed Control, VIDEOS, BLDC Motors, Washdown, Application Examples, Medical, Food & Packaging, Grip Conveyors, Conveyors, Factory Automation

Minimize Conveyor Footprint with Right Angle Brushless Gear Motors

Posted by Johann Tang on Oct 1, 2018, 8:31:15 AM

Parallel shaft AC gear motors are the standard configuration in the industry.  However, right angle brushless gear motors are gaining popularity for their ability to minimize the footprint of a machine, such as a conveyor.  

Read More

Topics: AC Motors, Speed Control, VIDEOS, BLDC Motors, Gearheads, Application Examples, Medical, Food & Packaging, Conveyors, Factory Automation

    Subscribe Here!