Engineering Notes by Oriental Motor

Welcome to Oriental Motor's "Engineering Notes" Blog:

Products and technology are only valuable when coupled with skilled people and services to support them. Since 1978, ORIENTAL MOTOR U.S.A. CORP. has been building a service and support system to better serve customers. It is our goal to provide the best product and service from the design phase, through the sale and beyond.

Our blog will feature:

  • Introduction to new products and technologies
  • Motion control basics and application examples
  • Tips for motor selection, programming, and troubleshooting

 

Minimizing the Effect of Load Fluctuations for Mixers

Posted by Johann Tang on Jun 30, 2020, 12:00:00 PM

The viscosity change in liquids can vary the torque required for mixing.  For AC asynchronous motors such as AC induction motors, the rated speed is affected by load torque fluctuations, which may cause inconsistency in the final product.  Is there a better motor for the job?

Read More

Topics: Speed Control, VIDEOS, BLDC Motors, Gearheads, Washdown, Application Examples

Monitor Your Machine Like a Traffic Light System

Posted by Johann Tang on Jun 19, 2020, 8:00:00 PM

For automated factories, motor failures mean lost production and lost revenue.  Being able to identify the specific issue in advance and its location is critical to maintaining production efficiency.  To be successful, extra sensors must be added to detect abnormalities.  There may be an easier way.

Read More

Topics: Stepper Motors, Alphastep Hybrid Control, Linear Actuators, VIDEOS, Network, Application Examples, Troubleshooting, Factory Automation

The Proper Way to Use a Gripper

Posted by Johann Tang on Mar 5, 2020, 5:11:16 PM

A gripper is typically an end effector that is installed at the end of a robotic arm or on a cartesian robot and can be used to grip parts in order to transfer them from one location to another.  However, there's more to it than just closing the jaws to pinch a part.  

Read More

Topics: Stepper Motors, Robotics, Absolute Positioning, Alphastep Hybrid Control, Linear Actuators, VIDEOS, Application Examples

Reactive vs Preventive vs Predictive Maintenance: Why Predictive Maintenance is Better

Posted by Johann Tang on Aug 20, 2019, 2:58:24 PM

Along with the advancement of industrial technology, maintenance methods of motion control components of a machine, such as motors, drives, and sensors, have also evolved.

Most of us still use the traditional "reactive" maintenancemethod in many aspects of life, such as replacing a dishwasher in your kitchen.  People don't buy a dishwasher until theirs doesn't work anymore.  Well, for factories that rely on consistent uptime for production, this wasn't the best strategy.  Realizing the need for improvement, maintenance personnel started to estimate life and replace motion control components before they failed.  This is called the "preventive" maintenancemethod, which also wasn't a perfect strategy for cost.  More recently, with the advancement of IIoT (Industrial Internet of Things) technologies and real-time availability of status data, another method was made possible - the "predictive" maintenance method.

Read More

Topics: Stepper Motors, Linear Actuators, VIDEOS, Network, Application Examples

How Easy Is It to Build a Robot?

Posted by Johann Tang on Jul 19, 2019, 8:31:19 PM

Robot adoption is increasing in many industries due to global efforts in reducing long term costs, maintaining quality, and freeing up time for humans to do "human" tasks.  For example, by using a robot to clean floors or restock shelves in a supermarket, human employees can spend more time helping or selling to their customers.  A company can either tap into this robotic trend by buying ready-made robots, or by making their own with less cost. 

If engineering resources are limited, selecting the right components can reduce the difficulty and time for building a robot.

Read More

Topics: Stepper Motors, Robotics, Absolute Positioning, Alphastep Hybrid Control, Linear Actuators, Motor Sizing, VIDEOS, Gearheads, Software, Application Examples

Benefits of an Absolute Rack and Pinion System Compared to Other Linear Motion Mechanisms

Posted by Johann Tang on Jul 2, 2019, 3:25:24 PM

There are many mechanisms that convert rotary motion of an electric motor to linear motion, such as belt/chain drives, screw drives, rack & pinion drives and even CAM drives.  Each mechanism offers advantages and disadvantages. Choosing the right technology can help increase load, speed, travel distance, or positioning accuracy.

Read More

Topics: Absolute Positioning, Alphastep Hybrid Control, Linear Actuators, VIDEOS, Vertical Lifts, Application Examples

Eliminate Motor Speed Fluctuations Caused By Input Voltage or Load Variance

Posted by Johann Tang on Jun 21, 2019, 6:57:39 PM

An AC motor can be simple to use, but its speed changes according to the size of the load or amount of voltage supplied.  For an application where keeping a uniform speed is important, there is another type of motor that can improve performance.

Read More

Topics: AC Motors, Speed Control, VIDEOS, BLDC Motors, Application Examples

Improving Stop Accuracy for Start/Stop Conveyors

Posted by Johann Tang on May 7, 2019, 1:32:29 PM

Are you using motors for a start/stop conveyor or similar application?  While AC motors are a common choice for conveyors, there is a unique speed control motor solution available that could improve stop accuracy as well as reduce footprint and cost of machine designs.

Read More

Topics: AC Motors, Stepper Motors, Speed Control, VIDEOS, Application Examples, Conveyors, Incremental Positioning, Factory Automation

Better Motor Alternatives for Variable Speed Pumps

Posted by Johann Tang on May 6, 2019, 8:03:26 PM

What motors do you use for pumps?  For variable speed pump applications that typically use 3-phase AC induction motors with variable frequency drives (VFDs), there is another type of motor that can transfer fluids more consistently and help reduce footprint.

Read More

Topics: AC Motors, Speed Control, VIDEOS, BLDC Motors, Pumps, Application Examples, Medical

Simple Method to Limit Motor Operation Range for Robotics Safety

Posted by Johann Tang on Apr 1, 2019, 2:09:05 PM

In the world of industrial robotics, there are several types of robots typically offering multiple axes of motion for tasks such as parts assembly, material handling, or pick and place operations.  These include articulated robots, cartesian/gantry robots, SCARA robots, and Delta robots.  Variations of end effectors such as grippers, welders or part rotators can be mounted on the end of the arm to perform different tasks.  Depending on number of axes or load capacity, costs can easily add up.  Limiting the operation range for these robotic axes of motion is an easy way to prevent costly problems or safety issues later.

Read More

Topics: Stepper Motors, Robotics, Absolute Positioning, Alphastep Hybrid Control, VIDEOS, Software, Application Examples

    Subscribe Here!